MCWB configuring both main and aux position/speed sensors give conflict in timer IRQHandler
When configuring both main and aux sensors (Quad encoder and Hall) it is necessary to assign them to different timers, for example Encoder: TIM2, Ch1:A15, Ch2: B3 and Hall: TIM3, Ch1:C6, Ch2:C7, Ch3:C8. This leads to conflict in define for IRQHandler as shown below:
/********** AUXILIARY HALL TIMER MOTOR 1 *************/
#define M1_HALL_TIM_PERIOD 65535
#define M1_HALL_IC_FILTER 14
#define SPD_TIM_M1_IRQHandler TIM2_IRQHandler
/********** AUXILIARY ENCODER TIMER MOTOR 1 *************/
#define M1_PULSE_NBR ( (4 * (M1_ENCODER_PPR)) - 1 )
#define M1_ENC_IC_FILTER 12
#define SPD_TIM_M1_IRQHandler TIM3_IRQHandler
The generated code for SPD_TIM_M1_IRQHandler does not support _both_ sensor types but generates different code for each sensor type when used separately.
How can this problem be solved?
Background: Our application uses an encoder with 0.01 degree resolution for positioning and a Hall sensor for velocity up to 10000 rpm (where the encoder cannot follow).
BR
Håkan