Skip to main content
SOfne.1
Associate II
March 10, 2021
Solved

Bug in Low-Level driver LL_SPI_ReceiveData8 for STM32L0, STM32L4, STM32L5 and possibly others

  • March 10, 2021
  • 6 replies
  • 2146 views

Affected driver libraries: STM32Cube_FW_L5_V1.4.0, STM32Cube_FW_L4_V1.16.0, STM32Cube_FW_L0_V1.11.2 and possibly other device driver libraries based on the same SPI peripheral

File: stm32yyxx_ll_spi.h (Replace yy by L5, L4, F0, ...)

Functions affected: LL_SPI_ReceiveData8

Bug: Current implementation performs a 16bit read access to DR register and then casts the result to 8 bits. This leads to unexpected behavior. For example STM32L5 supports data packing, when SPI data frame size is less than or equal to 8 bits and 16 bits are read. In this case, the current implementation of LL_SPI_ReceiveData8 reads two (packed) bytes from DR register and discards the second one when casting the read result to 8 bits.

Correct implementation: Cast pointer to DR register to uint8_t before access.

__STATIC_INLINE uint8_t LL_SPI_ReceiveData8(SPI_TypeDef *SPIx)

{

  return *((__IO uint8_t *)&SPIx->DR)

}

This topic has been closed for replies.
Best answer by SOfne.1

Hi @Imen DAHMEN​ 

Thank you.

As you can see in the corresponding git repository for STM32CubeF0 firmware package this issue is still present in STM32CubeF0 V1.11.2.

Best regards,

Sebastian

6 replies

ST Technical Moderator
March 10, 2021

Hello @SOfne.1​  and welcome to the STM32 Community :)

Thanks for pointing out this issue.

I am checking it internally and I will come back to you with details about corrective actions we will take, or explanation if needed.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
March 18, 2021

​Hi @SOfne.1​ ,

This issue will be fixed in the coming release of STM32CubeL5 MCU package.

Thanks for your contribution.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
SOfne.1
SOfne.1Author
Associate II
March 22, 2021

Hi @Imen DAHMEN​ 

Thanks for your fast response. Will this issue be fixed in the next releases of STM32CubeF0 and STM32CubeL4 MCU package, too?

Best regards,

Sebastian

ST Technical Moderator
March 25, 2021

Hi @SOfne.1​,

You are right, only LL_SPI_TransmitData8() is correct in the latest CubeF0. I've escalated this issue to correct LL_SPI_ReceiveData8() API.

The same correction will be performed for all impacted series.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks