Skip to main content
SPark.28
Associate II
March 8, 2021
Solved

Is it possible to trigger serially using timers.

  • March 8, 2021
  • 3 replies
  • 990 views

For example, there are 3 timers (Timer 1, 2, 3).

I want to set like below:

  • Timer 1 : Master
  • Timer 2 : Slave of Timer1
  • Timer 3 : Slave of Timer2

When I checked the waveform after setting similarly to the above, it seemed that timer2 could not trigger timer3 properly.

So, I wonder if it is possible to trigger serially using timers.​

This topic has been closed for replies.
Best answer by waclawek.jan

The easiest way is to read them out in the debugger.

If you don't use debugger, then write a function which outputs their content to an UART, or similar.

JW

3 replies

waclawek.jan
Super User
March 8, 2021

> timer2 could not trigger timer3 properly

Why do you think so?

Read out and check/post content of timers registers.

JW

SPark.28
SPark.28Author
Associate II
March 9, 2021

I want to know method to read out registers.

waclawek.jan
waclawek.janBest answer
Super User
March 9, 2021

The easiest way is to read them out in the debugger.

If you don't use debugger, then write a function which outputs their content to an UART, or similar.

JW