Skip to main content
dungeonlords789
Associate III
March 7, 2021
Question

CubeProg 2.6 is unstable

  • March 7, 2021
  • 10 replies
  • 3477 views

CubeProg 2.6.0 is very unstable!

I use it to program (upgrade FUS, stack) my stm32WB55 on MB1293C board and sometimes when I push buttons CubeProg is closing.

Windows 7.

0693W000008wDwBQAU.png0693W000008wDwLQAU.png

This topic has been closed for replies.

10 replies

dungeonlords789
Associate III
March 10, 2021

@Imen DAHMEN​ 

ST Technical Moderator
March 11, 2021

Hello @dungeonlords789​ ,

Thanks for pointing out to me this issue.

I raised your feedback internally to be reviewed and treated by our expert accordingly to the priority.

I'll make sure to post updates here as soon as I have more details.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
dungeonlords789
Associate III
March 12, 2021

I also recomend make text more userful

1) "Firmware delete" - what should do this button? Delete firmware on MCU1, MCU2, both, or delete FUS? May be it should calls "Radio stack delete"?

2) "Start adress". I thing it should be a list, not text edit. It is not userfull because you allow write any number...

3) "Verify download" Are you sure that user can decide verify or not? Of cause flash must be verified! So I think you should remove this checkbox and verify after every writing.

4) What means "full chip erase" button in case of stm32wb55? Erase MCU1, MCU2, FUS, all? In CubeProg 2.6 this button just fail:

01:04:01 : MASS ERASE ...

01:04:01 : Error: Mass erase operation failed.Please verify flash protection

01:04:01 : Warning: Connection to device 0x495 is lost

01:04:02 : Disconnected from device.

Khouloud OTHMAN
Associate
April 5, 2021

Hello @dungeonlords789​ ,

First let me thank you for your feedback and for the useful suggestions you gave, they will be taken into consideration.

Sorry for the late update :grinning_face_with_sweat:, but I wasn't able to reproduce the issue from my side.

Could you please re-test with the latest STM32CubeProgrammer version 2.7.0 and check if this issue still persists ?

I'll be waiting for you feedback.

Khouloud.

LMI2
Senior III
April 5, 2021

Well, You are lucky, I can't close mine.

Khouloud OTHMAN
Associate
April 6, 2021

Hi  @LMI2​ ,

Do you mean that by pressing the Firmware delete button, STM32CubeProgrammer crashes and could not be closed anymore ? did I will understand your problem?

Also, could you please precise which board are you using as well as the STM32CubeProgrammer version you're working with.

Your feedback will be very important to track the root cause of any misbehavior.

Khouloud.

LMI2
Senior III
May 1, 2021

I updated the CubeProgrammer and tested my board today, and I did not find any problems.

Thank you for your support

LMI2
Senior III
May 1, 2021

Ah. I am sorry, I didn't notice your reply. I'll report when I am using the again. Thank you for your help.