Shutdown mode wakeup does not works in STM32WB
Hi,
I am using STM32WB55CG nucleo board. I wrote a program as follows.
- Reset the device
- run BLE sequencer for 1 minute ( advertise BLE for i minute)
- read the time and date
- save the time and date in flash
- enter shutdown mode
- Wakeup from shutdown mode (using RTC wakeup) in every 10s and execute 3,4 and 5 steps
shutdown mode wake up does not works. But when I remove the second step in the program wakeup is working. After integrating the BLE in to the code wakeup does not works. My program as follows. Can anyone help me ?
if( (__HAL_PWR_GET_FLAG(PWR_FLAG_C2SB) == RESET)
)
{
APPE_Init();
BLE_MODE =1;
}
while(BLE_MODE){
UTIL_SEQ_Run(~0);
if(HAL_GetTick()>60000){
BLE_MODE=0;
}
}
while(1){
HAL_RTC_GetTime(&hrtc, &time_struct_t, RTC_FORMAT_BIN);
HAL_RTC_GetDate(&hrtc, &date_struct_t, RTC_FORMAT_BIN);
temperature_value = Get_Temperature();
log_data(date_struct_t,time_struct_t,temperature_value);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_SET);
HAL_Delay(20);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_RESET);
Enter_shutdownMode();
}