Skip to main content
FaikN
Associate III
March 3, 2021
Question

STM32G0/G4 Accessory Debug Mode Firmware: Is it supported/ implemented within the USB PD firmware?

I have been using STM32G MCUs with USB PD Sink or Source application. Right now, I want to implement Debug Accessory Mode in either STM32G0 or G4 MCUs with SInk USB PD Application. Hence, i would like to use USB-C cable SBU and Data lines for MCU flashing.

When i created an example project and inspected the firmware, i found out that the SNK_ACCESORY is not defined and it is not within and cinfig file, even though i checked the box of CAD Debug within CubeIDE. When i inspected further, i found out in usbpd_def.h that the CAD_AccesorySupport is commented as not yet implemented. I would like to see if i can implement the Debug Accesory Mode by manually defining the SNK_ACCESSORY.

What are the steps i need to follow to implement this mode within STM PD3 Stack? Is there any further example project i can follow from one of these MCUs for Debug Accessory Mode application?

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    March 3, 2021
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    FaikN
    FaikNAuthor
    Associate III
    March 3, 2021

    yeah my mistake, added to USB-PD tagged sub-forum. will delete this one.