Skip to main content
Ankyt
Visitor II
March 3, 2021
Question

What will be the status of the CMOD bit in the OTG_GINTSTS register when no USB device is connected to the port?

  • March 3, 2021
  • 0 replies
  • 474 views

I am using the NUCLEO-L4R5ZI-P development board for testing OTG. My use-case is with OTG is a USB Disk as an MSC device with STM32 as a host and PC as a Host with STM32 as a CDC device.

I follow the steps which are given in the user manual of STM32L4+ MCUs for the OTG_FS programming model. So how can I check whether there is any device available or not?

Thanks,

Ankit

This topic has been closed for replies.