Skip to main content
ACHAB.1
Visitor II
February 25, 2021
Question

What is the best way to backup some bytes whitout RTC backup registers in order to enter in shutdown mode.

  • February 25, 2021
  • 1 reply
  • 563 views

Hello, I use STM32L476 for very low power project. I also use an external RTC because it is temperature-compensated. My question is : What is the best way to backup some bytes whitout RTC backup registers in order to enter in shutdown mode.

I had the idea to use internal flash memory but I need to backup some dozen of bytes. I need to do the same task about ten times before read all of these bytes and delete them. Because of erasing before writing, I consider that flash isn't the best way.

If anyone can help me, I'll be awsome.

Thanks in advance

Chabot Axel

This topic has been closed for replies.

1 reply

Uwe Bonnes
Chief
February 25, 2021

There are a lot of ap notes and threads about using flash as EEPROM.