Skip to main content
fulcrumEFX
Associate II
February 24, 2021
Question

Bug in CMSIS V2 Layer in combination with C++ project (FreeRTOS+LwIP)

  • February 24, 2021
  • 2 replies
  • 4328 views

Hello,

When creating a C++ Project for STM32F7 (my Board: Nucleo F767Zi) with LwIP and FreeRTOS with CMSIS V2 Layer, after 30 seconds up to a few minutes Ethernet communication stops working (Stuck in cmsis_os2.c at xSemaphoreTake (hMutex, timeout) ).

Steps to recreate the Bug:

  • Create new STM32 Project for Nucleo F767Zi with targeted language C++ (CubeIDE 1.5.1 with STM32Cube_FW_F7_V1.16.0)
  • In CubeMX change Systick to TIM6, enable LwIP and FreeRTOS with CMSIS V2
  • Build and flash Board
  • continuously ping the board and wait for it to crash

See also my previous post: https://community.st.com/s/question/0D53W00000aqa2WSAQ/freertos-lwip-in-c-project-on-stm32f7

It works if I either:

  • convert Project to C in CubeIDE
  • switch to CMSIS V1

Greetings

This topic has been closed for replies.

2 replies

Visitor II
June 22, 2023

I encountered the same bug two years later
LWIP works on my stm32f7 using cmsis_v1 but not with cmsis_v2
any update?

Associate II
February 23, 2024

I am facing same issue while creating a C project with STM32F746 Discovery board with Ethernet and FreeRTOS, I am able to ping to my board when I use CMSIS v1 but not the case when I am using CMSIS v2.

I am following this tutorial  

I am able to run TCP, UDP on baremetal code but I am having difficulties using FreeRTOS 

I have attached CbueMX report and source code for TCP suing netconn and my main.c  fiel.