Question
UART - Data corruption due to noisy receive line
I found out in the errata of STM32G070 MCU (page: 12, section: 2.11.1) that: in UART mode with oversampling by 8 or 16 and with 1 or 2 stop bits, the received data may be corrupted if a glitch to zero shorter than the half-bit occurs on the receive line within the second half of the stop bit.
Workaround
None.
My UART configuration:
Baud Rate: 460800
Word Length: 8bits
Stop bits: 1
Oversampling: 16
- Does this mean that if the stop bit goes zero during its second half (due to some glitch/noise), then, the data maybe corrupted?
- If so, how frequently can this occur if my application uses a FTDI TTL USB to UART cable to communicate with PC with some serial terminal (ex. Putty) ?
- Also, does changing the stop bits resolve this issue? The MCU supports 0.5 & 1.5 stop bits as well. Though some serial terminals doesn't seem to support non integer stop bits.
Thanks