Skip to main content
NAwari
Associate II
February 18, 2021
Question

Is it possible to use S2LP transceiver IC with pulse interval encoding (PIE) other than Manchester and NRZ encoding schemes mentioned in the datasheet?

  • February 18, 2021
  • 6 replies
  • 1314 views

..

    This topic has been closed for replies.

    6 replies

    Winfred LU
    ST Employee
    February 18, 2021

    PIE is not supported natively as far as i understand.

    A possible option is to use the mode direct through GPIO, which the data will send directly to and/or receive directly from some GPIO.

    But the controller (MCU) has to deal with the encoding/decoding.

    NAwari
    NAwariAuthor
    Associate II
    February 18, 2021

    If I understood you correctly, then one should do the encoding/decoding at MCU and send the encoded data for modulation to the S2LP IC? Does that mean one has to build a logic/circuit to convert data into PIE encoded data?

    Winfred LU
    ST Employee
    February 19, 2021

    Right. It is because PIE is not supported.

    To achieve the needed (unsupported) encoding schemes, the user may try to encode/decode manually, by customizing the data through GPIO.

    NAwari
    NAwariAuthor
    Associate II
    February 20, 2021

    Can then one use PWM output pins of STM32L152RE MCU to generate required encoding and then send data through GPIO to the encoder (where no inbuilt encoder is used) and pass it through modulation block?

    I believe it is possible to disable all the encoding and decoding schemes from S2LP IC. Can you please comment on it?

    Winfred LU
    ST Employee
    February 23, 2021

    >Can then one use PWM output pins of STM32L152RE MCU to generate required encoding

    Maybe. I don't have the answer now.

    The challenge here is that PWM encodes data into different duty cycles (%) but a single bit 0 and 1 both take the same amount of time,

    however, PIE has different amount of time between 0 and 1.

    NAwari
    NAwariAuthor
    Associate II
    February 23, 2021

    Can you please also comment on "I believe it is possible to disable all the encoding and decoding schemes from S2LP IC?"