Skip to main content
KiptonM
Senior III
February 16, 2021
Solved

What keystrokes are needed to change the Pin that MX selects for a peripheral?

  • February 16, 2021
  • 1 reply
  • 752 views

I have the Nucleo-F446RE. And when I ran the MX it set USART3_TX to Pin PB10. Looking at table 11 in DS10693 Rev 10 STM32F446xC/E

It says

USART3_TX can be on PB10, PC10, and PD8.

It looks like PD8 is not on the STM32F446 Nucleo-64 board.

PB10 is on CN9-7 and CN10-25

PC10 is on CN7-1

How do I tell the USART3 Mode and Configuration -> GPIO Settings to use PC10 and not PB10?

No combination of keystrokes/mouse clicks let me change it that I know of.

This topic has been closed for replies.
Best answer by Khouloud ZEMMELI

Hello @KiptonM​ 

Thanks for your question,

In fact, the PD8 is only available on LQFP144 , UFBGA144 and LQFP100 packages as mentioned in the DataSheet, for that, the STM32F446RE which has the LQFP64 package, the USART3_TX signal cannot be assigned to PD8 pin.

Now, if you want to use the PC10 as pin for the USART3_TX signal, you have just to click on PC10 and choose the USART3_TX (before the activation of the USART IP or even after).

0693W000008GNZ8QAO.png 

I would like to take this opportunity to present you another way to know the possible Pins that can be remapped instead of other pins for a signal used, without referring to DS and directly through the Pinout view of the CubeMX interface, you need just to put the cursor on pin (which has already a signal on it) and press CTRL+Click, then CubeMX will give you all possible pins which contain the same signal (Alternates) :

0693W000008GNXDQA4.png 

Hope my answer helped you, when your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thanks for your contribution, Khouloud

1 reply

Khouloud ZEMMELI
Khouloud ZEMMELIBest answer
ST Employee
February 17, 2021

Hello @KiptonM​ 

Thanks for your question,

In fact, the PD8 is only available on LQFP144 , UFBGA144 and LQFP100 packages as mentioned in the DataSheet, for that, the STM32F446RE which has the LQFP64 package, the USART3_TX signal cannot be assigned to PD8 pin.

Now, if you want to use the PC10 as pin for the USART3_TX signal, you have just to click on PC10 and choose the USART3_TX (before the activation of the USART IP or even after).

0693W000008GNZ8QAO.png 

I would like to take this opportunity to present you another way to know the possible Pins that can be remapped instead of other pins for a signal used, without referring to DS and directly through the Pinout view of the CubeMX interface, you need just to put the cursor on pin (which has already a signal on it) and press CTRL+Click, then CubeMX will give you all possible pins which contain the same signal (Alternates) :

0693W000008GNXDQA4.png 

Hope my answer helped you, when your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thanks for your contribution, Khouloud