Skip to main content
NBruh.1
Associate
February 13, 2021
Question

Touch GFX 4.16 - Code generation bricking project

  • February 13, 2021
  • 6 replies
  • 1309 views

I have been having issues with Touch GFX bricking my project during code generation. It starts out working but at a later point it starts generating invalid code. An example is that it starts generating a touchgfx::GraphElementLine without a variable name. Another example is it cannot find certain fonts cpp files during compilation. I can e.g. fix the GraphElementLine by deleting my dynamicGraph and creating a new one. The font issue I haven't found a solution for. Anyone else experienced this and know how to fix it?

This topic has been closed for replies.

6 replies

Romain DIELEMAN
ST Employee
February 18, 2021

Hi,

Did you find a solution to your problem ? The font issue is intriguing, could you share a project where you face this ? What kind of fonts are they ?

Are you working on a custom hardware or with an application template for one of the ST development kits ?

And sorry but could you explain to me what you mean by bricking :grinning_face_with_sweat: ? I personally use that term when a project completely crashes and the hardware can be used as a paperweight ;) (so useless). Is it what you mean as well or am I an uncultured swine ?

/Romain​

DOS
Visitor II
February 18, 2021

I have met the same issue regarding "cannot find certain fonts cpp" with TouchGFX 4.16.

I just followed the official tutorial 2 step by step.

The error occurs after adding the range "0-9" in the "Wildcard Ranges" column for the Default typography.

 Compiling generated/fonts/src/Table_verdana_10_4bpp.cpp
 g++: error: generated/fonts/src/Font_verdana_40_4bpp_0.cpp: No such file or directory
 g++: fatal error: no input files
 compilation terminated.
 g++: error: generated/fonts/src/Table_verdana_80_4bpp.cpp: No such file or directory
 g++: fatal error: no input files
 compilation terminated.
 g++: error: generated/fonts/src/GeneratedFont.cpp: No such file or directory
 g++: fatal error: no input files
 compilation terminated.

0693W000008GYoxQAG.png    

I checked the files under generated/fonts/src/ dictionary, all above mentioned files exist.

I did the same tutorial 2 with TouchGFX 4.15, it works fine.

I also compared generated files from two different TouchGFX Designer, they are identical.

​ My board : STM32H747-DISCO

Romain DIELEMAN
ST Employee
February 18, 2021

The application templates for the H747 boards are a bit apart from the others because the ATs are quite old now and are not based on STM32CubeMX (because CubeMX does not support dual cores and additional softwares). I have reported the issue but I) can only advise to continue using 4.15 until this is fixed. (maybe look at the makefile in the gcc folder to see the call for those files)

/Romain

NBruh.1
NBruh.1Author
Associate
February 18, 2021

And for what I mean by bricking is that if I manually fix the naming of the touchgfx::GraphElementLine then when I run the simulator through touchgfx then it will automatically regenerate the code overwriting my manual fix :grinning_face_with_sweat: