Skip to main content
Javier1
Principal
Feb 11, 2021 3:41 PM UTC
Solved

Flashing empty memory pages with cubemx locks my mcu

Good evening stm32 dwellings, i have a flash problem.

I find myself with the need to write a config file independent to my programm code.

In order to do that my programm uses pointers to specific memory pages of my stm32f105:

define ADDR_FLASH_PAGE_54 ((uint32_t)0x0801B000) /* Base @ of Page 54, 2 Kbytes */
#define ADDR_FLASH_PAGE_55 ((uint32_t)0x0801B800) /* Base @ of Page 55, 2 Kbytes */

For debugging purposes i created a temporal setup function that writes the a hardcoded config structure directly to my flash. (<- this is working fine, reading and writting)

BUT

Once i build my own configFile.bin and try to flash it with stm32cubeMX i get this:

 0693W000007EwP0QAK.png 

the flashed data looks fine when i read the memory, but the mcu is locked, once i start a debugging session it goes into hardfault at random moments.

this is the verbosity output of the stm32cubeMX flashing

I have no idea of what is going on....

16:38:55:746 : Memory Programming ...
 16:38:55:756 : Opening and parsing file: archivobinario_pointerArray.bin
 16:38:55:757 : File : archivobinario_pointerArray.bin
 16:38:55:757 : Size : 120 Bytes
 16:38:55:757 : Address : 0x0801B000 
 16:38:55:757 : Erasing Segment <0> Address <0x0801B000> Size <120>Bytes
 16:38:55:758 : Erasing memory corresponding to segment 0:
 16:38:55:760 : Memory erase...
 16:38:55:760 : halt ap 0 
 16:38:55:760 : w ap 0 reg 15 PC (0x20000000) 
 16:38:55:760 : w ap 0 reg 17 MSP (0x20000500) 
 16:38:55:760 : w ap 0 reg 16 xPSR (0x01000000) 
 16:38:55:763 : w ap 0 @0x20000960 0x00000200 bytes Data 0x00000000
 16:38:55:767 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00
 16:38:55:783 : w ap 0 @0x20000004 0x0000053E bytes Data 0xF000B580
 16:38:55:790 : Erasing internal memory sector 54
 16:38:55:791 : Init flashloader...
 16:38:55:792 : halt ap 0 
 16:38:55:792 : w ap 0 reg 0 R0 0x00000001
 16:38:55:793 : w ap 0 reg 1 R1 0x00000000
 16:38:55:793 : w ap 0 reg 2 R2 0x00000000
 16:38:55:793 : w ap 0 reg 3 R3 0x00000000
 16:38:55:793 : w ap 0 reg 4 R4 0x00000000
 16:38:55:794 : w ap 0 reg 5 R5 0x00000000
 16:38:55:795 : w ap 0 reg 6 R6 0x00000000
 16:38:55:795 : w ap 0 reg 7 R7 0x00000000
 16:38:55:795 : w ap 0 reg 8 R8 0x00000000
 16:38:55:796 : w ap 0 reg 9 R9 0x00000000
 16:38:55:797 : w ap 0 reg 10 R10 0x00000000
 16:38:55:798 : w ap 0 reg 11 R11 0x00000000
 16:38:55:799 : w ap 0 reg 12 R12 0x00000000
 16:38:55:804 : w ap 0 reg 13 SP 0x00000000
 16:38:55:805 : w ap 0 reg 14 LR 0x20000001
 16:38:55:805 : w ap 0 reg 15 PC 0x20000005
 16:38:55:805 : w ap 0 reg 16 xPSR 0x01000000
 16:38:55:805 : w ap 0 reg 17 MSP 0x2000093E
 16:38:55:805 : w ap 0 reg 18 PSP 0x00000000
 16:38:55:805 : run ap 0 
 16:38:55:806 : halt ap 0 
 16:38:55:806 : r ap 0 reg 0 R0 0x00000001
 16:38:55:806 : Loader sector erase...
 16:38:55:806 : w ap 0 reg 0 R0 0x0801B000
 16:38:55:806 : w ap 0 reg 1 R1 0x0801B000
 16:38:55:808 : w ap 0 reg 2 R2 0x00000002
 16:38:55:808 : w ap 0 reg 3 R3 0x00000000
 16:38:55:808 : w ap 0 reg 4 R4 0x00000000
 16:38:55:808 : w ap 0 reg 5 R5 0x00000000
 16:38:55:808 : w ap 0 reg 6 R6 0x00000000
 16:38:55:808 : w ap 0 reg 7 R7 0x00000000
 16:38:55:808 : w ap 0 reg 8 R8 0x00000000
 16:38:55:808 : w ap 0 reg 9 R9 0x00000000
 16:38:55:809 : w ap 0 reg 10 R10 0x00000000
 16:38:55:809 : w ap 0 reg 11 R11 0x00000000
 16:38:55:809 : w ap 0 reg 12 R12 0x00000000
 16:38:55:809 : w ap 0 reg 13 SP 0x00000000
 16:38:55:809 : w ap 0 reg 14 LR 0x20000001
 16:38:55:810 : w ap 0 reg 15 PC 0x200001AF
 16:38:55:812 : w ap 0 reg 16 xPSR 0x01000000
 16:38:55:812 : w ap 0 reg 17 MSP 0x2000093E
 16:38:55:813 : w ap 0 reg 18 PSP 0x00000000
 16:38:55:813 : run ap 0 
 16:38:55:868 : halt ap 0 
 16:38:55:868 : r ap 0 reg 0 R0 0x00000001
 16:38:55:868 : erase: 0069ms
 16:38:55:869 : Download in Progress:
 16:38:55:869 : Size : 120 Bytes
 16:38:55:869 : Address : 0x0801B000 
 16:38:55:869 : Buffer program...
 16:38:55:870 : halt ap 0 
 16:38:55:870 : w ap 0 reg 15 PC (0x20000000) 
 16:38:55:870 : w ap 0 reg 17 MSP (0x20000500) 
 16:38:55:870 : w ap 0 reg 16 xPSR (0x01000000) 
 16:38:55:871 : w ap 0 @0x20000960 0x00000200 bytes Data 0x00000000
 16:38:55:871 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00
 16:38:55:877 : w ap 0 @0x20000004 0x0000053E bytes Data 0xF000B580
 16:38:55:877 : Loader write range...
 16:38:55:878 : w ap 0 @0x20000960 0x0000003C bytes Data 0x0801B800
 16:38:55:878 : W B1 in RAM @0x20000960 size 0x0000003C : 0002ms
 16:38:55:878 : Init flashloader...
 16:38:55:878 : halt ap 0 
 16:38:55:878 : w ap 0 reg 0 R0 0x00000001
 16:38:55:878 : w ap 0 reg 1 R1 0x00000000
 16:38:55:879 : w ap 0 reg 2 R2 0x00000000
 16:38:55:879 : w ap 0 reg 3 R3 0x00000000
 16:38:55:879 : w ap 0 reg 4 R4 0x00000000
 16:38:55:879 : w ap 0 reg 5 R5 0x00000000
 16:38:55:879 : w ap 0 reg 6 R6 0x00000000
 16:38:55:879 : w ap 0 reg 7 R7 0x00000000
 16:38:55:879 : w ap 0 reg 8 R8 0x00000000
 16:38:55:879 : w ap 0 reg 9 R9 0x00000000
 16:38:55:880 : w ap 0 reg 10 R10 0x00000000
 16:38:55:880 : w ap 0 reg 11 R11 0x00000000
 16:38:55:880 : w ap 0 reg 12 R12 0x00000000
 16:38:55:881 : w ap 0 reg 13 SP 0x00000000
 16:38:55:882 : w ap 0 reg 14 LR 0x20000001
 16:38:55:882 : w ap 0 reg 15 PC 0x20000005
 16:38:55:883 : w ap 0 reg 16 xPSR 0x01000000
 16:38:55:884 : w ap 0 reg 17 MSP 0x2000093E
 16:38:55:887 : w ap 0 reg 18 PSP 0x00000000
 16:38:55:887 : run ap 0 
 16:38:55:887 : halt ap 0 
 16:38:55:887 : r ap 0 reg 0 R0 0x00000001
 16:38:55:888 : w ap 0 reg 0 R0 0x0801B000
 16:38:55:888 : w ap 0 reg 1 R1 0x0000003C
 16:38:55:888 : w ap 0 reg 2 R2 0x20000960
 16:38:55:888 : w ap 0 reg 3 R3 0x00000002
 16:38:55:888 : w ap 0 reg 4 R4 0x00000000
 16:38:55:889 : w ap 0 reg 5 R5 0x00000000
 16:38:55:889 : w ap 0 reg 6 R6 0x00000000
 16:38:55:890 : w ap 0 reg 7 R7 0x00000000
 16:38:55:890 : w ap 0 reg 8 R8 0x00000000
 16:38:55:890 : w ap 0 reg 9 R9 0x00000000
 16:38:55:890 : w ap 0 reg 10 R10 0x00000000
 16:38:55:890 : w ap 0 reg 11 R11 0x00000000
 16:38:55:891 : w ap 0 reg 12 R12 0x00000000
 16:38:55:891 : w ap 0 reg 13 SP 0x00000000
 16:38:55:891 : w ap 0 reg 14 LR 0x20000001
 16:38:55:891 : w ap 0 reg 15 PC 0x2000002F
 16:38:55:891 : w ap 0 reg 16 xPSR 0x01000000
 16:38:55:891 : w ap 0 reg 17 MSP 0x2000093E
 16:38:55:891 : w ap 0 reg 18 PSP 0x00000000
 16:38:55:891 : run ap 0 
 16:38:55:892 : w ap 0 @0x2000099C 0x0000003C bytes Data 0x0801B800
 16:38:55:892 : W B2 in RAM @0x20008360 size 0x0000003C: 0027ms
 16:38:55:892 : r ap 0 reg 0 R0 0x00000001
 16:38:55:892 : Wait W B1 in Flash @0x0801B000 size 0x0000003C: 0001ms
 16:38:55:893 : w ap 0 reg 0 R0 0x0801B03C
 16:38:55:893 : w ap 0 reg 1 R1 0x0000003C
 16:38:55:894 : w ap 0 reg 2 R2 0x2000099C
 16:38:55:894 : w ap 0 reg 3 R3 0x00000002
 16:38:55:894 : w ap 0 reg 4 R4 0x00000000
 16:38:55:894 : w ap 0 reg 5 R5 0x00000000
 16:38:55:895 : w ap 0 reg 6 R6 0x00000000
 16:38:55:895 : w ap 0 reg 7 R7 0x00000000
 16:38:55:896 : w ap 0 reg 8 R8 0x00000000
 16:38:55:897 : w ap 0 reg 9 R9 0x00000000
 16:38:55:898 : w ap 0 reg 10 R10 0x00000000
 16:38:55:899 : w ap 0 reg 11 R11 0x00000000
 16:38:55:899 : w ap 0 reg 12 R12 0x00000000
 16:38:55:901 : w ap 0 reg 13 SP 0x00000000
 16:38:55:901 : w ap 0 reg 14 LR 0x20000001
 16:38:55:903 : w ap 0 reg 15 PC 0x2000002F
 16:38:55:903 : w ap 0 reg 16 xPSR 0x01000000
 16:38:55:903 : w ap 0 reg 17 MSP 0x2000093E
 16:38:55:903 : w ap 0 reg 18 PSP 0x00000000
 16:38:55:903 : run ap 0 
 16:38:55:904 : r ap 0 reg 0 R0 0x00000001
 16:38:55:904 : Write elapsed time: 0042ms
 16:38:55:904 : Segment[0] downloaded successfully
 16:38:55:905 : File download complete
 16:38:55:924 : Time elapsed during download operation: 00:00:00.130
 16:38:55:924 : RUNNING Program ... 
 16:38:55:924 : Address: : 0x0801B000
 16:38:55:934 : w ap 0 reg 15 PC 0x0801B858
 16:38:55:936 : w ap 0 reg 17 MSP 0x0801B800
 16:38:55:939 : w ap 0 reg 16 xPSR 0x01000000
 16:38:55:940 : Warning: The core is locked up
 16:38:55:954 : Start operation achieved successfully

Extra ball: if i do full chip erase and then i flash again my small config file at start address 0x0801B000 i also get the Warning: The core is locked up

This topic has been closed for replies.
Javier1
Javier1Best answer
Principal
Apr 24, 2023 10:20 PM UTC

I did overcome this issue purely by ignoring It.

I Believe the core is locked Up message showed Up because cubeprogrammer was tryingto run the binary file right after flashing.

​

As It was just raw config data not compiled Code , thus it was crashing​

hit me up in https://www.linkedin.com/in/javiermuñoz/

2 replies

CCend.2
Associate II
Apr 24, 2023 5:38 PM UTC

I'm having the same issue when flashing my chip using STM32CubeProgrammer. Were you ever able to fix it?

Javier1
Javier1AuthorBest answer
Principal
Apr 24, 2023 10:20 PM UTC

I did overcome this issue purely by ignoring It.

I Believe the core is locked Up message showed Up because cubeprogrammer was tryingto run the binary file right after flashing.

​

As It was just raw config data not compiled Code , thus it was crashing​

hit me up in https://www.linkedin.com/in/javiermuñoz/