2021-02-19 6:58 PM
Hi everyone, we have a problem using LPTIM4 PWM output on STM32H747I-DISCO when system enters STOP mode.
In this project, I need two independent PWM outputs with fixed frequency to work, while system goes to STOP mode to save power. LPTIM1_OUT & LPTIM4_OUT are used for this purpose.
■ The issue is:
1.In RUN mode, both LPTIM PWM works as expected.
2. After system enters STOP mode, LPTIM1_OUT keeps PWM output, as expected.
But LPTIM4_OUT PWM stopped.
3. When system wakes up from STOP mode, LPTIM4 starts PWM generation again automatically. This behavior seems like normal timer, not low-power timer.
■ The waveform shown below helps to demonstrate the issue:
Red - LPTIM1_OUT
Yellow - LPTIM4_OUT
Green - MCU current consumption
■ Configuration codes are generated by STM32CubeIDE.
Some code excerpts:
A. Clock Source of LPTIM1 & LPTIM4 are LSE:
PeriphClkInitStruct.Lptim1ClockSelection = RCC_LPTIM1CLKSOURCE_LSE;
PeriphClkInitStruct.Lptim345ClockSelection = RCC_LPTIM345CLKSOURCE_LSE;
B. LPTIM init Functions
// ------------------------ LPTIM Init Functions ----------------------------
static void MX_LPTIM1_Init(void)
{
hlptim1.Instance = LPTIM1;
hlptim1.Init.Clock.Source = LPTIM_CLOCKSOURCE_APBCLOCK_LPOSC;
hlptim1.Init.Clock.Prescaler = LPTIM_PRESCALER_DIV1;
hlptim1.Init.Trigger.Source = LPTIM_TRIGSOURCE_SOFTWARE;
hlptim1.Init.OutputPolarity = LPTIM_OUTPUTPOLARITY_LOW;
hlptim1.Init.UpdateMode = LPTIM_UPDATE_IMMEDIATE;
hlptim1.Init.CounterSource = LPTIM_COUNTERSOURCE_INTERNAL;
hlptim1.Init.Input1Source = LPTIM_INPUT1SOURCE_GPIO;
hlptim1.Init.Input2Source = LPTIM_INPUT2SOURCE_GPIO;
if (HAL_LPTIM_Init(&hlptim1) != HAL_OK)
{
Error_Handler();
}
}
static void MX_LPTIM4_Init(void)
{
hlptim4.Instance = LPTIM4;
hlptim4.Init.Clock.Source = LPTIM_CLOCKSOURCE_APBCLOCK_LPOSC;
hlptim4.Init.Clock.Prescaler = LPTIM_PRESCALER_DIV1;
hlptim4.Init.Trigger.Source = LPTIM_TRIGSOURCE_SOFTWARE;
hlptim4.Init.OutputPolarity = LPTIM_OUTPUTPOLARITY_LOW;
hlptim4.Init.UpdateMode = LPTIM_UPDATE_IMMEDIATE;
hlptim4.Init.CounterSource = LPTIM_COUNTERSOURCE_INTERNAL;
if (HAL_LPTIM_Init(&hlptim4) != HAL_OK)
{
Error_Handler();
}
}C. Start PWM generation:
HAL_LPTIM_PWM_Start(&hlptim1, 32767, 16383);
HAL_LPTIM_PWM_Start(&hlptim4, 32767, 16383);
D. To enter system STOP mode:
HAL_PWREx_ConfigD3Domain(PWR_D3_DOMAIN_STOP);
HAL_PWREx_EnterSTOPMode( PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFI, PWR_D3_DOMAIN);
HAL_PWREx_EnterSTOPMode( PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI, PWR_D1_DOMAIN);
Solved! Go to Solution.
2021-02-20 12:07 AM
Sorry, this issue has been fixed after adding these two lines in LPTIM4_Init:
__HAL_RCC_LPTIM4_CLKAM_ENABLE();
__HAL_RCC_LPTIM4_CLK_SLEEP_ENABLE();
This requirement is described in RM0399, P.408:
"In order for the LPTIMER to operate with lse_ck or lsi_ck when the circuit is in STOP mode, the user application has to select the lsi_ck or lse_ck input via LPTIMxSEL fields, and set bit LPTIMxAMEN and LPTIMxLPEN to '1'."
** LPTIMxLPEN is enabled by default, while 'LPTIM1AMEN' does not exist since it is not located in D3 domain.
2021-02-20 12:07 AM
Sorry, this issue has been fixed after adding these two lines in LPTIM4_Init:
__HAL_RCC_LPTIM4_CLKAM_ENABLE();
__HAL_RCC_LPTIM4_CLK_SLEEP_ENABLE();
This requirement is described in RM0399, P.408:
"In order for the LPTIMER to operate with lse_ck or lsi_ck when the circuit is in STOP mode, the user application has to select the lsi_ck or lse_ck input via LPTIMxSEL fields, and set bit LPTIMxAMEN and LPTIMxLPEN to '1'."
** LPTIMxLPEN is enabled by default, while 'LPTIM1AMEN' does not exist since it is not located in D3 domain.
2021-02-25 5:30 AM
Hello @RChie.2 and thanks for sharing the solution.
I marked your answer as "Best Answer", this can be very helpful for Community users to find this solution more quickly.
Imen