Skip to main content
VRaja.3
Visitor II
February 8, 2021
Question

Reading from L9663 PSI5 Transceiver

  • February 8, 2021
  • 1 reply
  • 695 views

Hello,

I am using L9663 PSI5 transceiver for the development of a steering drive project. I have a doubt regarding the SPI communication. If I want to read a register content will I be able to get it in the same MISO data?

For example, I am sending a 32-bit SPI data (MOSI) to read the content in register "SR1". Can I get the data in the received SPI frame (MISO)?

Please clarify.

Best Regards

Varun R

    This topic has been closed for replies.

    1 reply

    AIsma.2
    Visitor II
    August 31, 2022

    Yes, this is the design of the SPI protocal to have a replsonse from MISO in the same transfer.