Skip to main content
nickagian
Associate
February 4, 2021
Question

Which compiler to use for BlueNRG-LP?

  • February 4, 2021
  • 1 reply
  • 764 views

Hi,

I am at a complete loss, so I would really appreciate any direction you could give me.

I have bought a STEVAL-IDB011V1 evaluation board for the BlueNRG-LP and I would like to edit / extend one of the example applications. But this is my first time ever with STM MCU products. My question is then, which compiler do I have to use here? I see in the user manual of the evaluation board the Keil and IAR are mentioned, but these require a paid license. Isn't it possible to use any free of charge compiler?

EDIT: I have tried using the Atollic TrueStudio, but apparently the BlueNRG-LP is still not supported. Can somebody confirm that? Any other option, apart from that?

/Nikos

This topic has been closed for replies.

1 reply

DSong.1743
Associate
February 9, 2021

Use KEIL, and it is free to use for all ST Devices embedding a Cortex-M0.

https://www2.keil.com/stmicroelectronics-stm32/mdk