2021-01-29 8:53 PM
Hello. I want to make the controller a slave for the SPI. I understand the hardware activation Support leg stm8 at present, as it was then activated receiving \ transmitting?
/* Includes ------------------------------------------------------------------*/
#include "stm8s.h"
/* Private defines -----------------------------------------------------------*/
#define TIM4_PERIOD 124
#define USER_TIME_CYCLE 10
unsigned int system_plc_time = USER_TIME_CYCLE;
bool Start_SPI = FALSE;
//bool Start_SPI = TRUE;
uint8_t system_buff_mb_msg_rx[10];
/* Private function prototypes -----------------------------------------------*/
static void CLK_Config(void);
static void TIM4_Config(void);
static void SPI_Config(void);
static void EXTI_Config(void);
/* Private functions ---------------------------------------------------------*/
static void CLK_Config(void)
{
CLK_DeInit();
CLK_HSICmd(ENABLE);
CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);
CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);
//CLK_CCOConfig(CLK_OUTPUT_MASTER);
}
static void TIM4_Config(void)
{
TIM4_DeInit();
TIM4_TimeBaseInit(TIM4_PRESCALER_128, TIM4_PERIOD);
TIM4_ClearFlag(TIM4_FLAG_UPDATE);
TIM4_ITConfig(TIM4_IT_UPDATE, ENABLE);
TIM4_Cmd(ENABLE);
TIM4_ClearITPendingBit(TIM4_IT_UPDATE);
}
static void SPI_Config(void)
{
SPI_DeInit();
SPI_Init(SPI_FIRSTBIT_MSB,
SPI_BAUDRATEPRESCALER_2,
SPI_MODE_SLAVE,
SPI_CLOCKPOLARITY_LOW,
SPI_CLOCKPHASE_1EDGE,
SPI_DATADIRECTION_2LINES_FULLDUPLEX,
SPI_NSS_SOFT,
0x07);
SPI_NSSInternalSoftwareCmd(DISABLE);
SPI_ITConfig(SPI_IT_RXNE, ENABLE);
//SPI_ITConfig(SPI_IT_WKUP, ENABLE);
SPI_Cmd(ENABLE);
}
static void EXTI_Config(void)
{
EXTI_DeInit();
GPIO_Init(GPIOA, GPIO_PIN_3, GPIO_MODE_IN_PU_IT);
EXTI_SetExtIntSensitivity(EXTI_PORT_GPIOA, EXTI_SENSITIVITY_FALL_LOW);
}
INTERRUPT_HANDLER(TIM4_UPD_OVF_IRQHandler, 23)
{
disableInterrupts();
system_plc_time--;
TIM4_ClearITPendingBit(TIM4_IT_UPDATE);
enableInterrupts();
}
INTERRUPT_HANDLER(SPI_IRQHandler, 10)
{
disableInterrupts();
//if (Start_SPI == TRUE)
//{
Start_SPI = FALSE;
//SPI_ITConfig(SPI_IT_RXNE, DISABLE);
system_buff_mb_msg_rx[0] = SPI_ReceiveData();
SPI_SendData(system_buff_mb_msg_rx[0]);
//}
enableInterrupts();
}
INTERRUPT_HANDLER(EXTI_PORTA_IRQHandler, 3)
{
disableInterrupts();
Start_SPI = TRUE;
//SPI_ITConfig(SPI_IT_RXNE, ENABLE);
enableInterrupts();
}
void main(void)
{
CLK_Config();
TIM4_Config();
SPI_Config();
EXTI_Config();
enableInterrupts();
/* Infinite loop */
while (1)
{
if(!system_plc_time)
{
//SPI_SendData(127);
system_plc_time = USER_TIME_CYCLE;
}
}
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval : None
*/
void assert_failed(u8* file, u32 line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* Infinite loop */
while (1)
{
}
}
#endifin code i rx/tx one byte for test