Documents for implementing motor serial communications class
- January 29, 2021
- 3 replies
- 6156 views
I'm implementing a motor control project using a STM32G431 device. The host computer will communicate to the MCU through an FPGA. Presently my thoughts are to implement the serial framing protocol on the host side and I am using this document: UM1052 User manual (STM32F PMSM single/dual FOC SDK v4.3) as a reference.
Is this document (2016) still applicable?
Edit: added file. The portion I'm interested in is Section 14. Whether this works impacts the PC code as well as the FPGA code.
As example I was thinking of having the PC GUI code issue 'SM1' to the FPGA UART to start the motor. The FPGA would then send 0x03 0x01 0x01 CRC to the MCU through the MCU UART. The FPGA will be connected to up to 4 MCU's, each with their own motor and UART interface.