B-G431B-ESC1 kit issues profiling motors
Hi ST,
I have tried unsuccessfully to profile two very distinctly different motors also with a broad range of settings.
From this post https://community.st.com/s/question/0D53W00000HwV8RSAV/bg431besc1-motor-profiler-not-working-moderator-note-this-post-contains-now-a-bugfix-patch-on-provided-example on the same topic, I understand there was an issue with a batch of boards which may have caused it. Despite examining the boards, I am unable to tell the revision number on them.
How can I tell what revision my boards are?
I have tried the 5.4.4 motor profiler (which I understand from the above post is faulty), the patched version of that profiler and 5.4.5, all without success.
The error I get most of the time is "... taking too long" just after 90%. I successfully get consistent albeit not necessarily accurate electrical parameters, but I fail to get output from the mechanical side of the testing.
I have also tried to take the electrical parameters and plug them into Motorware. I then generated the code for the default example for the B-G431B-ESC1 and compiled the software. Unfortunately, this consistently led to "speed feedback" erros on the Motorware console, which makes me believe that this may be caused by faulty hardware.
Is there perhaps something else I'm missing here?
Thank you for your assistance.