Question with editing linker file (variable stored in flash)
Hello! I was trying to set aside a section in flash for a variable (I do have a reason to be doing so but, for the time being, I'm in the learning process to make sure I understand how it works before I do anything (too) stupid).
Anyway, my chip was the STM32L412RB. I am currently setting it up so I can set aside the last 16 bytes of flash for a variable location that I'm calling FLASH_ARRAY.
I managed to get it to recognize the last 16 bytes of flash for the variable, so that part looks good. Here is my code
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 40K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 128k-16
FLASH_VAR (rx) : ORIGIN = 0x801FFF0, LENGTH = 16
}So far, all looks good and it's assigning the section 16 bytes in this section in the Memory Details section in STM32CubeIDE.
The problem comes when I'm trying to assign a specific location within this section (say I want to assign a specific variable inside this location, for instance). Below is effectively how I want to assign a variable, for instance (below is only one variable but, I could potentially add multiple variables in this section).
uint8_t flash_array[16]
__attribute__((section(".flash_var .FLASH_ARRAY")));If I understand what I'm seeing on another example (as I'm seeing at this location: https://stackoverflow.com/questions/58256229/stm32f0-how-do-i-assign-values-from-variables-in-ram-to-a-separate-variable ), this can potentially be done with the following added to the "SECTIONS" section:
.flash_var :
{
KEEP(*(.flash_var .FLASH_ARRAY))
*(.flash_var *);
} > FLASH_VARWhen I try and run this though, I get the following errors:
section `.flash_var' will not fit in region `FLASH_VAR'
`FLASH_VAR' overflowed by 947837 bytesClearly, I set that last section up wrong, since the errors are introduced when I add that in. Since I don't seem to assign the variable a specific location (or size), I assume it's defaulting to a significantly larger size? I originally thought it might've been related to the min heap (0x200) or stack size (0x400) but that doesn't make sense in this context, from what I can see.
Could even be that I can't declare a section in flash smaller than a flash page size (which I need to look up, actually, that could be it). I found something regarding there being 64 pages of 2 kb programming. Does this mean I need to have sections that are all at least 2 kB? 64 pages of 2 kb would be 128 kb, so that does make sense . . .
EDIT: Ok, I tried the following and I'm getting the same errors, so I guess it's not that . . .
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 40K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 126k
FLASH_VAR (rx) : ORIGIN = 0x801E000, LENGTH = 2k
}Any idea what might be going on here? I believe I'm close but I'm not quite there yet. Any info you can give me would be appreciated. Thanks!