Question
I-NUCLEO-LRWAN1 and STM32F767ZI problem with usart
Hi, I'm working on the Lora project. I have a STM32F767ZI board and an I-NUCLEO-LRWAN1 module. As I understood from the manual to the module. The module is programmed using AT commands via UART. I set up USART3 on my board to communicate with a PC that works properly. I set up USART6 in the same way to send commands to the module. But when I try to send something to USART6 (speed 115200) my STM32 restarts. I will be happy for any idea.Or if someone was dealing with something similar, I would like to be inspired. Thank you