I need the definition of NTC_GetAvTemp_d() to calculate a float value of the temperature
I've been using (int32_t)NTC_GetAvTemp_C(pTemperatureSensor[0]) to read temperature but the draw back is that it is in integer deg C, I'd like a float with at least 1 digit resolution., i.e. 38.2. I'd like to use NTC_GetAvTemp_d() but don't know the definition. It is returning an int16_t value. Around 38C I get back a value of 17600.
This is what I know about the procedure:
/**
* @brief Returns latest averaged temperature measured expressed in u16Celsius
* @p pHandle : Pointer on Handle structure of TemperatureSensor component
* @r AverageTemperature : Current averaged temperature measured (in u16Celsius)
*/
__weak uint16_t NTC_GetAvTemp_d( NTC_Handle_t * pHandle )
{
return ( pHandle->hAvTemp_d );
}Can someone tell how to interpret "u16Celsius" ?
Note: Since I have the NTC coefficients I could write my own routine but I was trying to use the available procedures without creating redundant code, not to mention reducing the software/ADC timing overhead.