Motor profiler does not connect NUCLEO-F746ZG and X-NUCLEO-IHM08M1 3Sh Workbench connects but cannot spin the motor
I am using the NUCLEO-F746ZG and X-NUCLEO-IHM08M1 3Sh configuration and try to run the motor Profiler. However, the programming seems to run properly, the connection to the board does not seems to work. I got the warning : The FW embeeded on control board is correct, but the control board communication is still missing.
I also run another test with the Workbench solution and manage to connect to the board but the motor is not spinning. I am not sure what I am missing. Regarding the configuration of the boards themselves, information I found really depend on the source for my combo. Despite a lot of tests, the result is always the same.
Hope you can help,
regards