Hello @TGoto.1 and welcome to the ST Community.
Both solution you mentioned are based on STSPIN32F0601 System-In-Package and fit your motor specification.
The main difference is in the shunt sensing topology:
- EVSPIN32F0601S1 has a single-shunt sensing topology. Both the field-oriented control (FOC) and sensored or sensorless 6‑step control can be implemented.
- EVSPIN32F0601S3 has a three-shunt sensing topology. The field-oriented control (FOC), either sensored or sensorless, can be implemented.
You can choose the board according to the driving method (FOC or 6-step) and shunt topology (single or three).
Let me know if these info are useful to you, if yes please "Select as Best" button to close the topic.