STM32F042 RTC wont start
I seem to be unable to get the RTC to start. I can set the time, and read from it, but it doesn't increment.
I have tried using the external and internal oscillator, neither have been successful.
Everything has been set up with CubeMx, and I have used the RTC before on an STM32L0 micro with no issue, comparing it to my old code I cant see what I am doing differently.
I have attached the relevant parts of the code, if you know what I am missing please let me know.
Thanks,
Luke
static void MX_RTC_Init(void)
{
RTC_TimeTypeDef sTime;
RTC_DateTypeDef sDate;
/**Initialize RTC Only
*/
hrtc.Instance = RTC;
if(HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR0) != 0x32F2){
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = 127;
hrtc.Init.SynchPrediv = 255;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Initialize RTC and set the Time and Date
*/
sTime.Hours = 0x0;
sTime.Minutes = 0x0;
sTime.Seconds = 0x0;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_RESET;
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
sDate.WeekDay = RTC_WEEKDAY_MONDAY;
sDate.Month = RTC_MONTH_JANUARY;
sDate.Date = 0x1;
sDate.Year = 0x0;
if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
HAL_RTCEx_BKUPWrite(&hrtc,RTC_BKP_DR0,0x32F2);
}
}
/* USER CODE BEGIN PV */
RTC_TimeTypeDef sTimeGet;
RTC_TimeTypeDef sTimeSet;
/* Private variables ---------------------------------------------------------*/
/* USER CODE END PV */
void updateTime(void){
//RTC_TimeTypeDef sTimeGet;
//RTC_TimeTypeDef sTimeSet;
HAL_RTC_GetTime(&hrtc, &sTimeGet, RTC_FORMAT_BIN);
seconds = sTimeGet.Seconds;
minutes = sTimeGet.Minutes;
hours = sTimeGet.Hours;
if(hours>12){
hours = 0;
sTimeSet.Hours = hours;
HAL_RTC_SetTime(&hrtc, &sTimeSet, RTC_FORMAT_BIN);
}
}