Using section attributes within a union
I've been assigning some of my storage areas into different memory areas as defined within the STM32H743ZITX_RAM.ld file in a project using STM32CubeIDE. This has first required me to insert the appropriate definitions where I've used memory domain D3 as an example:
MEMORY
{
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K
}
/* Sections */
SECTIONS
/* snip .. */
.myD3memory (NOLOAD):
{
. = ALIGN(4);
*(.myD3memory)
. = ALIGN(4);
} >RAM_D3
/* etc .. */
}I can then utilize this in main() as follows:
uint16_t buffer16[32768] __attribute__ ((section(".myD3memory")));This works exactly as I intended and Build Analyzer shows the correct allocation. However, I now have a new case where I would like to reference the memory area not just as 16-bit unsigned shorts but also 8-bit unsigned bytes and have tried the following:
union
{
uint8_t buffer8[65536] __attribute__ ((section(".myD3memory")));
uint16_t buffer16[32768] __attribute__ ((section(".myD3memory")));
}which unfortunately produces the errors:
../Core/Src/main.c: error: section attribute not allowed for 'buffer8'
uint8_t buffer8[65536] __attribute__ ((section(".myD3memory")));
^~~~~~~~~~~
../Core/Src/main.c: error: section attribute not allowed for 'buffer16'
uint16_t buffer16[32768] __attribute__ ((section(".myD3memory")));
Hopefully this will be an easy suggestion from someone more (GCC?) compiler savvy and any help in moving this forward would be greatly appreciated.