Question
Single use resources not being deleted when no longer used?
I have an application where all the texts are taken from (non-single use) resources. However I still have many (100s) of single use resources in my project from before I converted the text to use a (non-single use) resource. The majority of these single use resources are "New Text". My understanding was these single use resources should be deleted automatically when no longer used.
Is this feature broken, or have I misunderstood?
Is there some way to manually tidy these no longer used single use resrouces?
Using TouchGFX Designer v4.15.0.