Associate
January 16, 2021
Solved
CubeIDE doesn't set the toolchain for STM32H7, but it does for other boards
- 2 replies
- 2549 views
Hello, maybe a newbie question but I just received my very first STM32 board (Nucleo H745ZI-Q) to learn embedded programming (mostly for fun and maybe for neuroscience applications in the future) and have been trying to generate code using the default settings in CubeIDE. The code generation goes smoothly using the default settings, but then in the project properties window, no toolchain is set for the generated project (attached screenshot) and I can't compile the code. However, Using the same IDE, I noticed that I can generate code for other boards like STM32F1, and In this case, the toolchain is set correctly and everything works fine.
Does CubeIDE 1.5.1 support Nucleo H7 series boards? Already tried re-installing the IDE.