Skip to main content
ADysh.1
Associate
January 16, 2021
Solved

Problem with new version STM32CubeIDE ver1.5.1 and STM32CubeMX ver6.1.1 (fatal error: usb_device.h: No such file or directory)

  • January 16, 2021
  • 10 replies
  • 8508 views

Before that there was STM32CubeIDE ver1.4.0 STM32CubeMX ver6.0.0 everything was fine.

Installed STM32CubeIDE ver1.5.1 and STM32CubeMX ver6.1.1, there was an error when connecting USB_DEVICE.

Tried creating a project from scratch with nothing but USB_DEVICE. Gives an error message.

What to do?

0693W000007BX7KQAW.png

This topic has been closed for replies.
Best answer by TDK

I took your IOC, hit generate code, loaded the project and hit build. It built fine. Win10, CubeIDE 1.5.1, CubeMX 6.1.1, latest HAL package.

I know it's frustrating. Sorry, good luck.

...
Finished building target: new_new_f407vet6.elf
 
arm-none-eabi-size new_new_f407vet6.elf 
arm-none-eabi-objdump -h -S new_new_f407vet6.elf > "new_new_f407vet6.list"
arm-none-eabi-objcopy -O binary new_new_f407vet6.elf "new_new_f407vet6.bin"
 text	 data	 bss	 dec	 hex	filename
 25584	 492	 7948	 34024	 84e8	new_new_f407vet6.elf
Finished building: default.size.stdout
 
Finished building: new_new_f407vet6.bin
Finished building: new_new_f407vet6.list

10 replies

TDK
January 16, 2021

Check your include directories

Project properties -> C/C++ Build -> Setting -> Tool Settings -> MCU GCC Compiler -> Include Paths

"If you feel a post has answered your question, please click ""Accept as Solution""."
ADysh.1
ADysh.1Author
Associate
January 16, 2021

Added everything. It didn't get any easier. Error again!

0693W000007BXRjQAO.pngI specifically looked at the settings on the old version. The settings on both the old and the new version are the same. But the new one doesn't work!

0693W000007BXRtQAO.png

TDK
January 16, 2021
Different error message. It sees the file now. The init function should be within main.c. Regenerate the code. If that doesn’t work, attach your IOC file.
"If you feel a post has answered your question, please click ""Accept as Solution""."
ADysh.1
ADysh.1Author
Associate
January 16, 2021

1) I'm launching a new version of STM32CubeIDE ver1.5.1 (STM32CubeMX ver6.1.1).

I indicate the directory with the old project on STM32CubeIDE ver1.4.0 STM32CubeMX ver6.0.0.

At startup it says: “The workspace was written with an older version. Continue and update workspace which may make it incompatible with older version? ".

0693W000007BXbyQAG.pngI click Continue.

An older version message appears.

0693W000007BXc8QAG.pngI click Continue.

The project opens and works as expected.

Settings in the photo.

0693W000007BXcDQAW.png2) I click to create a new project.

I indicate the same chip.

USB only settings in virtual com port mode.

I generate a project.

Checking - again the same error!

Attach the IOC file.

Half a day was wasted. The new version does not work as expected out of the box. Very upset. I roll back to STM32CubeIDE ver1.4.0 STM32CubeMX ver6.0.0. Extremely disappointed.

Thank you for helping me. But this is beyond my strength.

My system: Windows 10 Pro, Lenovo ThinkPad T590 laptop. All updates have been installed.

TDK
TDKBest answer
January 16, 2021

I took your IOC, hit generate code, loaded the project and hit build. It built fine. Win10, CubeIDE 1.5.1, CubeMX 6.1.1, latest HAL package.

I know it's frustrating. Sorry, good luck.

...
Finished building target: new_new_f407vet6.elf
 
arm-none-eabi-size new_new_f407vet6.elf 
arm-none-eabi-objdump -h -S new_new_f407vet6.elf > "new_new_f407vet6.list"
arm-none-eabi-objcopy -O binary new_new_f407vet6.elf "new_new_f407vet6.bin"
 text	 data	 bss	 dec	 hex	filename
 25584	 492	 7948	 34024	 84e8	new_new_f407vet6.elf
Finished building: default.size.stdout
 
Finished building: new_new_f407vet6.bin
Finished building: new_new_f407vet6.list

"If you feel a post has answered your question, please click ""Accept as Solution""."
ADysh.1
ADysh.1Author
Associate
January 16, 2021

Thanks for the answer. Now I will know that the problem is on my side.

Good luck.

O'li
Associate II
January 22, 2021

Did you manage to solve your problem?

I had something similar and I suspect the code generation to not go all the way to the end: in your project's screenshot there's an "mx.scratch" file leftover, which should disappear once the code is generated.

Then, CubeMX might not generate/include all the driver files such as your usb_device.h one.

I managed to get rid of it by re-doing all the project creation from the *.ioc file. It worked for some time but it happens again, and it's quite laborious to re-do everything...

ADysh.1
ADysh.1Author
Associate
January 22, 2021

Hello.

No. The problem could not be resolved. I am working on version 1.4.

I even rolled back Windows to the old version, when I didn't have the CubeIDE program. Actually installed CubeIDE v1.5 from scratch.

And when creating a project, the same error came out!

Java is the latest version.

I tried to install Java of a different version, and noticed that a new error related to the usb library popped up. I didn't understand. The strength was gone.

IPaku.1
Visitor II
June 8, 2022

I had exactly the same problem with CubeIDE 1.9.0 and was stuck. Then I thought it'd be great to see some codegen logs, as it seems like codegen fails, since mx.scratch file stays in the project after codegen completes. That basically means there was something wrong with codegen.

So I though of that CubeIDE seems eclipse based, so I googled where eclipse's logs are, and they turn out to be in the workspace folder, under ".metadata' folder

In the logs I saw a weird error

!ENTRY com.st.stm32cube.common.mx 4 0 2022-06-08 16:42:07.293
!MESSAGE Error on line 9 of document file:/C:/STM32CubeIDE/workspace_1.9.0/another-try/mx.scratch: Invalid byte 2 of 2-byte UTF-8 sequence.
!STACK 0
org.jdom.input.JDOMParseException: Error on line 9 of document file:/C:/STM32CubeIDE/workspace_1.9.0/another-try/mx.scratch: Invalid byte 2 of 2-byte UTF-8 sequence.
	at org.jdom.input.SAXBuilder.build(SAXBuilder.java:530)
	at org.jdom.input.SAXBuilder.build(SAXBuilder.java:905)
	at org.jdom.input.SAXBuilder.build(SAXBuilder.java:884)

So I looked into mx.scratch file, line 9

And that line is specifying Firmware installation repository path. And that path has my name spelled in cyrillic.

So I went on to change the repository path, which you can do using "Window -> Preferences -> STM32Cube -> Firmware Updater -> Firmware installation repository"

You might as well want it fixed for CubeMX, "Help -> Updater Settings -> Repository Folder"

I changed it to "C:\ST\Repository"

Changing it as you might have guessed would not move the files, but it will redownload everything next time you try to build or codegen.

If this doesn't help, maybe you could further look into the logs file for clues..

Good luck with that :grinning_face:

MGare.1
Visitor II
July 8, 2022

Hi!

I had the same problem with CubeIDE 1.9.0. I was looking for the solution for several hours until I saw the suggestion of @IPaku.1​ and finally I could solve the problem. In order to solve it I did the following:

Inside the CubeIDE I went to "Window -> Preferences -> STM32Cube -> Firmware Updater"

0693W00000QKl9YQAT.pngIf you have the same problem, it is probably because at some point you changed the address of "Firmware installation repository". I say this because when I had done that, the problem started.

The solution was click on "Restore Defaults" then "Apply and Close" and finally create a new project.

0693W00000QKlBjQAL.pngI hope you can solve it too. Good luck!