Associate III
January 13, 2021
Solved
Output Compare differences between TIM1 and TIM8 in STM32F767
- January 13, 2021
- 3 replies
- 1635 views
Hello.
I want to use TIM8 instead of TIM1 to drive a WS2812B Led Strip together with DMA2 in STM32F767ZI. The code works fine with TIM1 but when I try to switch to TIM8 (which should have the same features), the interrupt handler TIM8_UP_TIM13_IRQHandler does not trigger anymore. Besides renaming everything from TIM1 to TIM8 I know I need to use TIM8_UP_TIM13 instead of TIM1_UP_TIM10 and also the strean/channel tie ins to the DMA2 also change. I have enclosed 2 pieces of code TIM1_WS2812B,c which works and TIM8_WS2812B.c where the TIM8 interrupt does not trigger. Aren't TIM1 and TIM8 suppose to work exactly the same way?
Thanks!