2021-01-13 1:34 AM
HRTIMe1 Interrupt needs HRTIM-MASTER Interrupt to fire?
I saw similar issue in GitHub but it pertains to Source of fault.
Anyway, I am using STM32G4 V1.3 on STMcubeIDE V1.5.1 on win10 machines (2 PCs)
It seems that HRTIM-E1 will not fire up the interrupt unless I enable HRTIM-MASTER and its interrupt via CubeMX.
Here is the setup of HRTIM-E1:
in main()
HAL_HRTIM_WaveformOutputStart(&hhrtim1, HRTIM_OUTPUT_TE1 );
HAL_HRTIM_WaveformCountStart_IT(&hhrtim1, HRTIM_TIMERID_TIMER_E );in MX_HRTIM1_Init()
static void MX_HRTIM1_Init(void)
{
/* USER CODE BEGIN HRTIM1_Init 0 */
/* USER CODE END HRTIM1_Init 0 */
HRTIM_TimeBaseCfgTypeDef pTimeBaseCfg = {0};
HRTIM_TimerCfgTypeDef pTimerCfg = {0};
HRTIM_CompareCfgTypeDef pCompareCfg = {0};
HRTIM_TimerCtlTypeDef pTimerCtl = {0};
HRTIM_OutputCfgTypeDef pOutputCfg = {0};
/* USER CODE BEGIN HRTIM1_Init 1 */
/* USER CODE END HRTIM1_Init 1 */
hhrtim1.Instance = HRTIM1;
hhrtim1.Init.HRTIMInterruptResquests = HRTIM_IT_NONE;
hhrtim1.Init.SyncOptions = HRTIM_SYNCOPTION_NONE;
if (HAL_HRTIM_Init(&hhrtim1) != HAL_OK)
{
Error_Handler();
}
if (HAL_HRTIM_DLLCalibrationStart(&hhrtim1, HRTIM_CALIBRATIONRATE_3) != HAL_OK)
{
Error_Handler();
}
if (HAL_HRTIM_PollForDLLCalibration(&hhrtim1, 10) != HAL_OK)
{
Error_Handler();
}
pTimeBaseCfg.Period = 27200;
pTimeBaseCfg.RepetitionCounter = 0x00;
pTimeBaseCfg.PrescalerRatio = HRTIM_PRESCALERRATIO_MUL8;
pTimeBaseCfg.Mode = HRTIM_MODE_CONTINUOUS;
if (HAL_HRTIM_TimeBaseConfig(&hhrtim1, HRTIM_TIMERINDEX_MASTER, &pTimeBaseCfg) != HAL_OK)
{
Error_Handler();
}
pTimerCfg.InterruptRequests = HRTIM_MASTER_IT_MREP;
pTimerCfg.DMARequests = HRTIM_MASTER_DMA_NONE;
pTimerCfg.DMASrcAddress = 0x0000;
pTimerCfg.DMADstAddress = 0x0000;
pTimerCfg.DMASize = 0x1;
pTimerCfg.HalfModeEnable = HRTIM_HALFMODE_DISABLED;
pTimerCfg.InterleavedMode = HRTIM_INTERLEAVED_MODE_DISABLED;
pTimerCfg.StartOnSync = HRTIM_SYNCSTART_DISABLED;
pTimerCfg.ResetOnSync = HRTIM_SYNCRESET_DISABLED;
pTimerCfg.DACSynchro = HRTIM_DACSYNC_NONE;
pTimerCfg.PreloadEnable = HRTIM_PRELOAD_DISABLED;
pTimerCfg.UpdateGating = HRTIM_UPDATEGATING_INDEPENDENT;
pTimerCfg.BurstMode = HRTIM_TIMERBURSTMODE_MAINTAINCLOCK;
pTimerCfg.RepetitionUpdate = HRTIM_UPDATEONREPETITION_ENABLED;
pTimerCfg.ReSyncUpdate = HRTIM_TIMERESYNC_UPDATE_UNCONDITIONAL;
if (HAL_HRTIM_WaveformTimerConfig(&hhrtim1, HRTIM_TIMERINDEX_MASTER, &pTimerCfg) != HAL_OK)
{
Error_Handler();
}
pCompareCfg.CompareValue = 5000;
if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_MASTER, HRTIM_COMPAREUNIT_1, &pCompareCfg) != HAL_OK)
{
Error_Handler();
}
if (HAL_HRTIM_TimeBaseConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_E, &pTimeBaseCfg) != HAL_OK)
{
Error_Handler();
}
pTimerCtl.UpDownMode = HRTIM_TIMERUPDOWNMODE_UP;
pTimerCtl.GreaterCMP1 = HRTIM_TIMERGTCMP1_EQUAL;
pTimerCtl.DualChannelDacEnable = HRTIM_TIMER_DCDE_DISABLED;
if (HAL_HRTIM_WaveformTimerControl(&hhrtim1, HRTIM_TIMERINDEX_TIMER_E, &pTimerCtl) != HAL_OK)
{
Error_Handler();
}
pTimerCfg.InterruptRequests = HRTIM_MASTER_IT_MREP;
pTimerCfg.DMARequests = HRTIM_TIM_DMA_NONE;
pTimerCfg.DMASrcAddress = 0x0000;
pTimerCfg.DMADstAddress = 0x0000;
pTimerCfg.DMASize = 0x1;
pTimerCfg.RepetitionUpdate = HRTIM_UPDATEONREPETITION_DISABLED;
pTimerCfg.PushPull = HRTIM_TIMPUSHPULLMODE_DISABLED;
pTimerCfg.FaultEnable = HRTIM_TIMFAULTENABLE_NONE;
pTimerCfg.FaultLock = HRTIM_TIMFAULTLOCK_READWRITE;
pTimerCfg.DeadTimeInsertion = HRTIM_TIMDEADTIMEINSERTION_DISABLED;
pTimerCfg.DelayedProtectionMode = HRTIM_TIMER_D_E_DELAYEDPROTECTION_DISABLED;
pTimerCfg.UpdateTrigger = HRTIM_TIMUPDATETRIGGER_NONE;
pTimerCfg.ResetTrigger = HRTIM_TIMRESETTRIGGER_NONE;
pTimerCfg.ResetUpdate = HRTIM_TIMUPDATEONRESET_DISABLED;
if (HAL_HRTIM_WaveformTimerConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_E, &pTimerCfg) != HAL_OK)
{
Error_Handler();
}
pCompareCfg.CompareValue = 10000;
if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_E, HRTIM_COMPAREUNIT_1, &pCompareCfg) != HAL_OK)
{
Error_Handler();
}
pOutputCfg.Polarity = HRTIM_OUTPUTPOLARITY_HIGH;
pOutputCfg.SetSource = HRTIM_OUTPUTSET_TIMPER;
pOutputCfg.ResetSource = HRTIM_OUTPUTRESET_TIMCMP1;
pOutputCfg.IdleMode = HRTIM_OUTPUTIDLEMODE_NONE;
pOutputCfg.IdleLevel = HRTIM_OUTPUTIDLELEVEL_INACTIVE;
pOutputCfg.FaultLevel = HRTIM_OUTPUTFAULTLEVEL_NONE;
pOutputCfg.ChopperModeEnable = HRTIM_OUTPUTCHOPPERMODE_DISABLED;
pOutputCfg.BurstModeEntryDelayed = HRTIM_OUTPUTBURSTMODEENTRY_REGULAR;
if (HAL_HRTIM_WaveformOutputConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_E, HRTIM_OUTPUT_TE1, &pOutputCfg) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN HRTIM1_Init 2 */
/* USER CODE END HRTIM1_Init 2 */
HAL_HRTIM_MspPostInit(&hhrtim1);
}in CubeMX
Period to set the IO and COMP1 to reset it
I have the output, but it will not enter the interrupt.
I use another I/O to check whether it entered or not.
void HRTIM1_TIME_IRQHandler(void)
{
/* USER CODE BEGIN HRTIM1_TIME_IRQn 0 */
GPIOC->BSRR = (1<<11); // start
/* USER CODE END HRTIM1_TIME_IRQn 0 */
HAL_HRTIM_IRQHandler(&hhrtim1,HRTIM_TIMERINDEX_TIMER_E);
/* USER CODE BEGIN HRTIM1_TIME_IRQn 1 */
GPIOC->BSRR = (1<<(11+16)); // end
/* USER CODE END HRTIM1_TIME_IRQn 1 */
}If I enable MASTER HRTIM but disable NVIC call handler
void HAL_HRTIM_MspInit(HRTIM_HandleTypeDef* hhrtim)
{
if(hhrtim->Instance==HRTIM1)
{
/* USER CODE BEGIN HRTIM1_MspInit 0 */
/* USER CODE END HRTIM1_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_HRTIM1_CLK_ENABLE();
/* HRTIM1 interrupt Init */
HAL_NVIC_SetPriority(HRTIM1_TIME_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(HRTIM1_TIME_IRQn);
/* USER CODE BEGIN HRTIM1_MspInit 1 */
/* USER CODE END HRTIM1_MspInit 1 */
}
}
The interrupt would fire up as shown below.
CH1 yellow = HRTIM-E1
CH2 green = PC11
What's more troubling is that the postion of the interrupt would depent on the HRTIM MASTER interrupt source.
In this case, CMP1 and repetition will fire up HRTIM-E1 (but not "timer update").
Also CMP1 of HRTIM-E1 will be used in case CMP1 as the source for HRTIM-MASTER.
Solved! Go to Solution.
2021-03-02 6:37 AM
2021-03-02 6:37 AM
2024-02-06 1:34 PM
Would you mind posting the answer? The link you posted doesn't work. All I get is this:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.