Skip to main content
SGada.1
Associate
January 13, 2021
Question

Is the X-NUCLEO-IHM08M1 inverter compatible with any STM32 NUCLEO board?

  • January 13, 2021
  • 0 replies
  • 414 views

Is the X-NUCLEO-IHM08M1 inverter compatible with any STM32 NUCLEO board?

Or is it only compatible with NUCLEO-F302R8 NUCLEO-F401RE?

In all the documentation I have seen it is used only with these boards. I need a better board such as the NUCLEO-H743ZI for my application. Before buying the parts I wanted to confirm if the X-NUCLEO-IHM08M1work with any STM32 NUCLEO board.

PS : When I say work with I mean, will it sit on the board correctly with the proper pins in the right place. Such as ADC pins of the MCU on the current sensing pins of the inverter.

Thanks!

This topic has been closed for replies.