Hello, I'm an electronic engineer and I'm working on a project for automation of agricultural machinery, we are using in this project the microcontroller STM32F446RCT7TR.
Hello, I'm an electronic engineer and I'm working on a project for automation of agricultural machinery, we are using in this project the microcontroller STM32F446RCT7TR. however I have little experience in this microcontroller and so I'm sorry if my question is a little obvious.
My question is, we are using an 8 MHz oscillator crystal with a large package in the prototype, but for the product I need to use an SMD crystal with the smallest possible package, which one would you recommend?
And because the application note AN2867 - Table 7 only indicates crystals of 32.7 MHz
Thanks