Skip to main content
BAher.1
Associate
January 7, 2021
Solved

STM32CubeMX on SPI2 set up

  • January 7, 2021
  • 2 replies
  • 1158 views

I am very new to the STM32 development board and am using the STM32F407VG. I wish to connect a RFID Scanner to SPI2 and looking at the Pin Description Table (pages 21->23 in the STM32F4 users manual), I cannot see if there are specific pins to be selected for SPI2 Chip-Select-Pin setup (I think I can use PB9 but am not sure). I think I'm correct to use SPI2->PC2 = MISO, SPI2->PC3 = MOSI & SPI2-> PB10 = CLK. Has anyone dealt with this issue that can help me to know if I have to select specific pin please?

This topic has been closed for replies.
Best answer by Khouloud OTHMAN

Hello BAher.1,

Welcome to our Community :)

You will find in the STM32F4 Data Sheet : Table 7. STM32F40xxx pin and ball definitions, specific pins for each peripheral.

Hope this answers your question.

If yes, please click on the Select as Best button on my reply . This will help other members of the community find this solution more quickly

Khouloud.

2 replies

Khouloud OTHMAN
Khouloud OTHMANBest answer
Associate
January 7, 2021

Hello BAher.1,

Welcome to our Community :)

You will find in the STM32F4 Data Sheet : Table 7. STM32F40xxx pin and ball definitions, specific pins for each peripheral.

Hope this answers your question.

If yes, please click on the Select as Best button on my reply . This will help other members of the community find this solution more quickly

Khouloud.

BAher.1
BAher.1Author
Associate
January 7, 2021

Thank you for the fast reply and all your help Khouloud =)