Skip to main content
pxueh.1
Associate II
January 6, 2021
Question

Multiple ADC sample with different frequency interference

  • January 6, 2021
  • 3 replies
  • 2114 views

Hi,everyone.I'm use NUCLEO-L496ZG platform.

ADC1 sample at a frequency of 5M,ADC3 sample at a frequency of 12.8K(PWM trigger).

when only run ADC3,ADC3's waveform is normal.

when ADC1 and ADC3 run at the same time,ADC3's waveform has a lot of interference.How to solve this problem? if had recommend frequency of ADC1 when ADC3 sample at a frequency of 12.8K? ADC1's frequency nend greater than 2M.

Time-domain waveform of ADC3(only ADC3 sample)

0693W000006HMT8QAO.png 

Time-domain waveform of ADC3(ADC3 and ADC1 sample together)0693W000006HMSyQAO.png 

Frequency spectrum waveform of ADC3(ADC3 and ADC1 sample together).

0693W000006HUpqQAG.pngThe follow picture is Enlarged view.(ADC3 and ADC1 sample together)

Input signal.

0693W000006HUqZQAW.pngInterference signal. The same of other three. Interval of frequency is 2560Hz

0693W000006HUqeQAG.png

3 replies

waclawek.jan
Super User
January 8, 2021

Do you sample the same signal by both ADCs?

What exactly is the circuitry at the input of both ADCs?

JW

pxueh.1
pxueh.1Author
Associate II
January 12, 2021

thanks for you reply, ADC1 and ADC3 is not sample the same signal, what ever ADC1 sample Any frequency even if ADC1 is grounding ,only ADC1 run, ADC3 has interference. Pulse signal generator output voltage into STM32 analog IO.(single-ended input)

Piranha
Principal III
March 28, 2021

The second image clearly shows that every n-th positive sample is 0 and every n-th negative sample is 1, which is probably because of some off-by-one processing error. Therefore look for wrong buffer address/size and flaws in processing code.

Visitor II
March 20, 2025

I want to know if you ultimately solved this problem, as I encountered the same issue on L496.