gpio let down 5 V pull-up
I use stm32f401's PB4 (NJTRST) pin. I attached 5 V pull-up resistor (5.1k) to PB4. While MCU is in reset mode the voltage on PB4 is 4.26 V. Only after starting the system, the voltage increases to 5 V. In my program I configure PB4 as input without pull-up or pull-down, just input. I couldn't find an explanation in AN4899.
Why voltage is 4.26 while reset? Is it because of schmitt trigger?