Associate II
January 1, 2021
Question
Custom Gauge background image not displaying correctly in TouchGFX Designer 4.16
- January 1, 2021
- 9 replies
- 4890 views
Hi,
I've just upgraded to version 4.16 of TouchGFX and noticed an issue with the new gauge widget.
When I use a custom background image it does not get displayed correctly inside the application. It's displayed somewhat "zoomed in". I've attached a screen shot showing the issue.
My background image is 112x112, and the widget is 112x112, however as you can see from the screenshot the image does not fit within the bounds of the widget.
It's worth noting that the image does render correctly on the actual target hardware (I haven't tried the simulator).
Is this a bug? Or have I missed one of the settings?
Thanks,
Simon