Reading from CAN bus (just as plain listener)
Hi ST Experts,
Recently I have started with experimentation on STM32407 Discovery board. Basically I am trying to implement CAN bus listener for particular ID from the vehicle. For my testing I am hooking on to OBD (where I have OBD unit to read the RPM, Speed etc). Here is the code snippet. Some how I am not getting any prints in my teraterm. Please let me know if you have any suggestions/ comments. I am using STM32CubeIDE with STM32Cube_FW_F4_V1.25.2 FW pack.
Helper functions are as below.
//for Raw OBD2 frame details
uint32_t FilterID = 0x7E8;
void CAN_FilterConfiguration(void)
{
CAN_FilterTypeDef CAN_RxFilter;
/* CAN filter configuration */
CAN_RxFilter.FilterActivation = ENABLE;
CAN_RxFilter.FilterBank = 0;
CAN_RxFilter.FilterFIFOAssignment = CAN_RX_FIFO0;
CAN_RxFilter.FilterIdHigh = FilterID << 5;
CAN_RxFilter.FilterIdLow = 0x000;
CAN_RxFilter.FilterMaskIdHigh = 0xFFE0;
CAN_RxFilter.FilterMaskIdLow = 0x000;
CAN_RxFilter.FilterMode = CAN_FILTERMODE_IDMASK;
CAN_RxFilter.FilterScale = CAN_FILTERSCALE_32BIT;
HAL_CAN_ConfigFilter(&hcan1, &CAN_RxFilter);
}
void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &FilterRxMessage, RxData);
my_printf("ID = 0x%x\n\r", FilterRxMessage.StdId);
my_printf("RTR = 0x%x\n\r", FilterRxMessage.RTR);
my_printf("DLC = 0x%x\n\r", FilterRxMessage.DLC);
my_printf("IDE = 0x%x\n\r", FilterRxMessage.IDE);
my_printf("RxData[0] = 0x%x, ", RxData[0]);
my_printf("RxData[1] = 0x%x, ", RxData[1]);
my_printf("RxData[2] = 0x%x, ", RxData[2]);
my_printf("RxData[3] = 0x%x, ", RxData[3]);
my_printf("RxData[4] = 0x%x, ", RxData[4]);
my_printf("RxData[5] = 0x%x, ", RxData[5]);
my_printf("RxData[6] = 0x%x, ", RxData[6]);
my_printf("RxData[7] = 0x%x, ", RxData[7]);
my_printf("\n\r");
//Re-start listening for CAN traffic with IT
HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING);
}
static void MX_CAN1_Init(void)
{
/* USER CODE BEGIN CAN1_Init 0 */
/* USER CODE END CAN1_Init 0 */
/* USER CODE BEGIN CAN1_Init 1 */
/* USER CODE END CAN1_Init 1 */
hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 6;
hcan1.Init.Mode = CAN_MODE_NORMAL;
hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan1.Init.TimeSeg1 = CAN_BS1_11TQ;
hcan1.Init.TimeSeg2 = CAN_BS2_2TQ;
hcan1.Init.TimeTriggeredMode = DISABLE;
hcan1.Init.AutoBusOff = DISABLE;
hcan1.Init.AutoWakeUp = DISABLE;
hcan1.Init.AutoRetransmission = DISABLE;
hcan1.Init.ReceiveFifoLocked = DISABLE;
hcan1.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan1) != HAL_OK)
{
my_printf ("CAN Init failed!!!!\n\r");
Error_Handler();
}
/* USER CODE BEGIN CAN1_Init 2 */
/* USER CODE END CAN1_Init 2 **/
}
In main () - I am calling
MX_CAN1_Init();
CAN_FilterConfiguration();
//Start listening for CAN traffic with IT
HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING);
and sit in while (1) loop. Basically I am trying to filter the message-ID - 7E8 which is very generic in OBD and I am expecting whenever I read the data from my OBD data (to which this CANH and CANL are hooked after transceiver) "HAL_CAN_RxFifo0MsgPendingCallback" should get called and I should be able to print the received data.
Do you have any comments/ suggestions for me?
With best regards,
Phani.