Skip to main content
DZhuy
Associate
December 26, 2020
Question

Stbc03. What will happen if IN voltage less than the battery voltage?

  • December 26, 2020
  • 4 replies
  • 1410 views

Hello, please help me understand:

1) What will happen if IN voltage less than the battery voltage? What voltage will in SYS in this case?

2) Сan I connect SYS pin to IN? I'ts safe?

This topic has been closed for replies.

4 replies

Winfred LU
ST Employee
December 29, 2020

1) shall not happen

Battery floating voltage is adjustable up to 4.45 V.

The minimum Vin will be 4.75 V when Vfloat is set to 4.45 V.

2) take your own risks

It means to skip the protections within STBC03.

DZhuy
DZhuyAuthor
Associate
December 29, 2020

Thanks for the answer. Can you please clarify one more question:

What if the battery is fully charged (4.2 V) and we supply 4.2 V or less( for example, 3.9 V) to the IN pin. In this case, what will be the voltage on the SYS pin?

Winfred LU
ST Employee
December 31, 2020

It will not work.

There is no grantee outside the range of operating input voltage : 4.45 V to 5.4 V

Cbalt.1
Associate II
February 17, 2024

Hello,

We could use STBC3 for stand alone application. I want to charge a mini battery as below specification. battery.jpeg 

 

I am planing to draw a pcb that contains USB socket and its power will  be come from 5V phone charger. May I use the STBC3  stand alone to charge this battery or should i put mcu to control charger limits. I confused. Previously I use TP4056 IC to chage higher capacity. It is the first time i am going to charge such a lower batter.  May you give some advise to me.

Best regards.