STM32G474 SPI DFU mode not working
I'm using STM32H753 eval board as master and STM32G474RE Nucleo board as slave over SPI1 communication. I've created a DFU for LED blink on Nucleo board which works fine if I download it through USB(connected PA11, PA12, 5V and GND) usinf DeFuseDemo tool. have set BOOT pin and all option bytes to enter into bootloader(system memory). If I connect it in SPI mode, I get ACK for all commands there is no single error in communication, all 5704 bytes from DFU file are written successfully. here is my code,
/* boot loader process starts */
blInit(&hspi1);
blGetCommand(spiRxBuffer);
version = blGetVersionCommand();
chipID = blGetIDCommand();
/* Check GetVersion is equal to GetCommand version */
if (version != spiRxBuffer[0])
{
/* TODO : exception handler */
}
/* Erase, write & verify loop #########################################*/
/* @note The Flash has to be erased before it can be written to */
/* (0x44) Erase Sector 0 (2 KBytes) */
blEraseMemoryCommand(0x0002, 0x00);
/* (0x31) Write firmware image */
if(blFWUpdateFlags.bUpdateImage)
{
copyImagefromFlash(devType, fname, buffer);
blFWUpdateFlags.bUpdateImage = 0;
}
uint8_t copyImagefromFlash(uint8_t devType, char *filename, uint8_t* buffer)
{
uint32_t len, temp;
if(lfs_file_open(&lfs, &slaveImageFile, filename, LFS_O_CREAT | LFS_O_RDWR | LFS_O_APPEND) != 0)
{
MPC_TRACE("\nSlaveFW.txt cannot be open\n");
return FILE_ERROR;
}
else
{
MPC_TRACE("\nSlaveFW.txt is open\n");
lfs_file_read(&lfs, &slaveImageFile, &dfuFilePrefix, ELEMENT_HEADER);
stDword(&slvElement.dwElementAddress, &dfuFilePrefix[3]);
stDword(&slvElement.dwElementSize, &dfuFilePrefix[7]);
//if(devType < STM32G07_DEV)
{
len = slvElement.dwElementSize;//(slaveImageFile.ctz.size - (OPTBYTE_STM32G47x + 8));
}
//else
//{
// len = (slaveImageFile.ctz.size - (OPTBYTE_STM32G07x + 8));
//}
len = (len / SLAVE_PAGEMEMORY_SIZE);
for (int i = 0; i < len; i++)
{
lfs_file_read(&lfs, &slaveImageFile, buffer, SLAVE_PAGEMEMORY_SIZE);
blWriteMemoryCommand(slvElement.dwElementAddress, SLAVE_PAGEMEMORY_SIZE, buffer);
slvElement.dwElementAddress += (SLAVE_PAGEMEMORY_SIZE);
}
len = slvElement.dwElementSize;
len = (len % SLAVE_PAGEMEMORY_SIZE);
lfs_file_read(&lfs, &slaveImageFile, buffer, len);
temp = (slaveImageFile.ctz.size - slvElement.dwElementSize);
if(devType < STM32G07_DEV)
{
if((temp) > (OPTBYTE_STM32G47x + 8))
{
temp = 1;
}
}
else
{
if((temp) > (OPTBYTE_STM32G07x + 8))
{
temp = 1;
}
}
if(temp == 1)
{
lfs_file_read(&lfs, &slaveImageFile, &dfuFilePrefix, ELEMENT_HEADER);
//stDword(&slvElement.dwElementAddress, &dfuFilePrefix[3]);
stDword(&slvElement.dwElementSize, &dfuFilePrefix[7]);
temp = (SLAVE_PAGEMEMORY_SIZE - len);
buffer = (buffer + len);
lfs_file_read(&lfs, &slaveImageFile, buffer, temp);
buffer = (buffer - len);
blWriteMemoryCommand(slvElement.dwElementAddress, SLAVE_PAGEMEMORY_SIZE, buffer);
slvElement.dwElementAddress += (SLAVE_PAGEMEMORY_SIZE);
len = slvElement.dwElementSize;
len = (len / SLAVE_PAGEMEMORY_SIZE);
for (int i = 0; i < len; i++)
{
lfs_file_read(&lfs, &slaveImageFile, buffer, SLAVE_PAGEMEMORY_SIZE);
blWriteMemoryCommand(slvElement.dwElementAddress, SLAVE_PAGEMEMORY_SIZE, buffer);
slvElement.dwElementAddress += (SLAVE_PAGEMEMORY_SIZE);
}
buffer = (buffer + len);
for (int i = len; i < SLAVE_PAGEMEMORY_SIZE; i++)
{
*buffer++ = 0xFF;
}
blWriteMemoryCommand(slvElement.dwElementAddress, SLAVE_PAGEMEMORY_SIZE, buffer);
}
else
{
buffer = (buffer + len);
for (int i = len; i < SLAVE_PAGEMEMORY_SIZE; i++)
{
*buffer++ = 0xFF;
}
blWriteMemoryCommand(slvElement.dwElementAddress, SLAVE_PAGEMEMORY_SIZE, buffer);
}
lfs_file_close(&lfs, &slaveImageFile);
return FILE_OK;
}
}Did anyone use DFU - SPI mode to update slave FW, would you please let me know where could be the issue.
thanks,