Skip to main content
WSart.1
Associate
December 24, 2020
Question

STM32L4 LPTIM as pulse counter of intermittent pulses fails when initialising with no pulse

  • December 24, 2020
  • 2 replies
  • 1521 views

I'm working with LPTIM as a Pulse Counter on a STM32L432KC, I have a rain gauge connected to LPTIM1 (PB5) and a anemometer to LPTIM2 (PB1). Both configured on STM32CubeMX as Standalone: counts external clock events and pins assigned as LPTIM?_IN1 using LSE clock.

To simplify, let's just use the anemometer but the symptoms is happening on the rain gauge as well.

Initializing the counter:

HAL_LPTIM_Counter_Start(&hlptim2, 0xffff);

This returns HAL_TIMEOUT when there's no pulse (no wind). If I turn the anemometer with my hand or is winding, when the device is initializing, it returns HAL_OK and it works just fine after that.

Troubleshooting, I found where it's timing out. On stm32l4xx_hal_lptim.c,, HAL_LPTIM_Counter_Start function, you can find this code:

 /* Load the period value in the autoreload register */
 __HAL_LPTIM_AUTORELOAD_SET(hlptim, Period);
 
 /* Wait for the completion of the write operation to the LPTIM_ARR register */
 if (LPTIM_WaitForFlag(hlptim, LPTIM_FLAG_ARROK) == HAL_TIMEOUT)
 {
 return HAL_TIMEOUT;
 }

There's application note AN4865 related to use LPTIM as a pulse counter and it doesn't say anything about LPTIM_ARR register neither LPTIM_ISR waiting for ARROK flag (4th bit). Also, on the example code, they expect a constant pulse signal arriving so this problem never happens.

If I comment if (LPTIM_WaitForFlag... block, it works perfectly.

I opened the issue on github: https://github.com/STMicroelectronics/STM32CubeL4/issues/24

This topic has been closed for replies.

2 replies

TDK
December 24, 2020

The reference manual explains the logic happening here.

0693W000006Gt1UQAS.png 

Code seems to be doing exactly what it should be doing, per the RM.

"If you feel a post has answered your question, please click ""Accept as Solution""."
WSart.1
WSart.1Author
Associate
December 24, 2020

To what I understand than, the if block commented can cause "unpredictable results".

Would you have a recommendation to my use case? I'm not by far an electronics specialist, it's just a hobby for me, and I ran out of ideas.

I thought on an extra pin attached to the anemometer pin, I bit-bang some pulses (or get another timer to generate a slow PWM), starts the LPTIM, stop the pulses after the successful start and I would be good to go. But I think this is a very ugly hack.