Using STM32F407G1-DISCO as a passive USB device to sniff on the bus.
I am using stm32f407g1-disco's High Speed USB core as a USB Device which has no class and is having an exernal ULPI PHY (USB3300) which is connected to the PC. On the other end of the USB3300 I have connected a USB VCP Device.
What I want to do is that let the PC and the USB VCP Device communicate with each other and the signals that I get on D+ and D- lines goes into both USB Devices(stm32f407 and USB VCP device) via USB3300 and I want to read those signals received in stm32f407's USB HS Controller via ULPI PHY but I don't know where that data gets stored at low level.
Could anyone please help me figure this out?
PS: when I monitor the D0:D7 lines of the stm32f407 by a logic analyzer which are connected to the external ULPI PHY, I am able to see the pulses coming on those lines which means that the signal is being received. Am I correct?