Skip to main content
CHeck.1
Associate II
Dec 18, 2020 7:21 AM UTC
Question

STM32G431 connect over JTAG

Hello,

I try to connect to a STM32G431 Device over JTAG. I got the following error. Has someone a solution for this error?

0693W000006GEUkQAO.png

This topic has been closed for replies.

10 replies

KnarfB
Super User
Dec 18, 2020 7:24 AM UTC

Did you upgrade to the latest tool version like STM32CuberProgrammer 2.6?

CHeck.1
CHeck.1Author
Associate II
Dec 18, 2020 7:38 AM UTC

Yes I am using V2.6

KnarfB
Super User
Dec 18, 2020 8:00 AM UTC

Custom board? Nucleo32 works here as expected. What probe?

CHeck.1
CHeck.1Author
Associate II
Dec 18, 2020 8:50 AM UTC

It is a self developed board. The JTAG connection works with an J-Link but not the ST-Link and STM32CubeProgrammer. Just a connection over SWD

KnarfB
Super User
Dec 18, 2020 9:39 AM UTC

Communication errors? You can lower the clock speed and re-check.

Uwe Bonnes
Chief
Dec 18, 2020 9:46 AM UTC

Firmware on the STLink recent? All STlink match JTAG ID against an internal list and reject parts they do not know(yet).

CHeck.1
CHeck.1Author
Associate II
Dec 18, 2020 9:50 AM UTC

Firmware on ST Link is recent

Uwe Bonnes
Chief
Dec 18, 2020 10:04 AM UTC

Does connect under reset work?

CHeck.1
CHeck.1Author
Associate II
Dec 18, 2020 10:22 AM UTC

No, it doesn't work

Uwe Bonnes
Chief
Dec 18, 2020 11:21 AM UTC

Double check your wiring, the problem is with 99.9% on your side. Get out the scope or LA and look at the signals.