Skip to main content
sryuj.1
Visitor II
December 18, 2020
Question

When using the STMF479, if the MIPI function is not used, can the corresponding pins be left unconnected?

  • December 18, 2020
  • 1 reply
  • 653 views

..

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
December 18, 2020

Yes, just leave the corresponding DSIHOST pins unconnected.

However, please note the information in the data sheet (Section 2.18).:

If DSI functionality is not used at all, then:

  • VDDDSI pin must be connected to global VDD.
  • VCAPDSI pin must be connected externally to VDD12DSI but the external capacitor is no more needed.
  • VSSDSI pin must be grounded

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.