Solved
STM32H7 - SPI : Activate the clock when i use the HAL_SPI_Receive_DMA method
Hello !
I'm trying to communicate with a ADC : AD7276. With my MCU STM32H745
To get the values from the ADC, I set the CS in low state and CLK 16 times.
However, the HAL_SPI_Receive_DMA method does not activate the clock on the SPI.
What are the parameters to activate the clock with this method?
I tried with the HAL_SPI_TransmitReceive_DMA method. But the first byte is missing ( while the byte in TX is transmited ).
I am in fullduplex and DMA TX/RX 8-ByteDataSize.
Thanks You :)