Skip to main content
DDomi.2
Visitor II
December 16, 2020
Question

STSPIN32F0 - Can I increase flash size?

  • December 16, 2020
  • 1 reply
  • 551 views

I'm working with this MCU in a project and ran out of flash space. Would like to know if there is a wat to add an external flash to this or if there is bigger flash option.

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
December 18, 2020

The STSPIN32F0 is based on the STM32F031C6, with the 32 KB flash already being the largest option. In addition to that it cannot be expanded externally due to the lack of an external bus interface. The STSPIN32F0 does contain an SPI interface, but it is neither suitable nor fast enough for executing code.

Have you already used the compiler option to improve optimization?

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.