Skip to main content
IShem.1
Associate
December 14, 2020
Question

STM32f103C8T6 BluePill external interrupt

  • December 14, 2020
  • 1 reply
  • 813 views

Hello, I am beginner and I am trying to write a code without HALL. The goal is switch LED when button press using interrupts. I check the button and the LED separately. Everything works fine. But interrupt code don't want to. What am I doing wrong? Using Keil5.

#include "stm32f10x.h" // Device header
 
static int temp = 0;
 
void EXTI0_IRQHandler(void)
{
	EXTI->PR |= 1 << 0;
	temp ^= 1;
}
 
int main()
{
	//initialize the clock for the GPIOC and GPIOA
	RCC->APB2ENR |= (1 << 4);
	RCC->APB2ENR |= (1 << 2);
	
	//configure pin 13 on GPIO C
	GPIOC->CRH |= ((1 << 20) | (1 << 21));	//output 50MHz
	GPIOC->CRH &= ~((1 << 22) | (1 << 23));	//general purpose output
	
	//configure button pin
	//GPIOA pin 0 input pullup
	GPIOA->CRL &= ~(1 << 1 | 1 << 0); 
	GPIOA->CRL |= 1 << 3;
	GPIOA->CRL &= ~(1 << 2);
	GPIOA->ODR |= 1 << 0;
	
	//configure interrupt
	RCC->APB2ENR |= RCC_APB2ENR_AFIOEN;
	AFIO->EXTICR[0] = AFIO_EXTICR1_EXTI0_PA;
	EXTI->FTSR |= 1 << 0;
	
	EXTI->IMR |= 1 << 0; //enable interrupt
	NVIC_EnableIRQ(EXTI0_IRQn); //
	NVIC_SetPriority(EXTI0_IRQn, 0);
	
	
	while(1)
	{
		if(temp)		
			GPIOC->BSRR = 1 << 13;
		else
			GPIOC->BSRR = 1 << (13 + 16);			
	}
		
	return 0;
}

This topic has been closed for replies.

1 reply

IShem.1
IShem.1Author
Associate
December 14, 2020

I don't know why, but after few hours of trying it suddenly start work. I haven't change the code that I wrote here. If it possible - delete this question. I am sorry.