2020-12-14 12:40 AM
Hello,
I am working with the evaluation board STM32L412 Nucluo64, but I noticed that the MCU sends only garbage from UART.
The code I am using has been used many times in other projects and should work fine (it's just a matter of calling LL_UART_TransmitData8 and wait for transfer complete).
Just tested on a STM32L4 Nucleo (STM32L432KC), same setup for both boards and works fine.
Do someone has an idea of what could be wrong ?
Thanks.
s.
Solved! Go to Solution.
2020-12-14 6:19 AM
Are you sure it uses a 25 MHz XTAL? Should use 8 MHz from ST-LINK or 32.768 KHz from LSE XTAL
Check HSE_VALUE define, and if you're using the MSI or HSI clock sources.
Availability and quality of baud rates will depend on available source clock.
2020-12-14 5:05 AM
Hello
STM32L412 NUCLEO uses 8 MHZ Clock from STLink as HSE
STM32L432KC NUCLEO uses 25 MHZ XTAL osc
2020-12-14 6:19 AM
Are you sure it uses a 25 MHz XTAL? Should use 8 MHz from ST-LINK or 32.768 KHz from LSE XTAL
Check HSE_VALUE define, and if you're using the MSI or HSI clock sources.
Availability and quality of baud rates will depend on available source clock.
2020-12-14 7:17 AM
Hello @Vangelis Fortounas ,
I think I don't understand at all your reply.
Nucleo64 jumper SB64 is open by default
The schematic correctly represents the real hardware connection.
HSI clock @16 MHz can be used with the PLL and getting a wide range of sys clock frequencies, smaller or greater than 25 MHz.
Using LL drivers, once set up the oscillator, the baudrate divider is automatically calculated into the function
LL_USART_SetBaudRatecalled from
LL_USART_InitWhat should be the difference from one clock frequency to another if both can achieve a correct divider for baudrate = 115200 ?
Thanks.
s.
2020-12-14 8:04 AM
MSI clock seems to work fine.
Thanks fot the hint.
s.
2020-12-14 9:29 AM
Hello, I was completely wrong about clocks. ( checked wrong schematics)
2020-12-14 9:39 AM
Hello .About the clocks , i was wrong(checked wrong schematics).
> What should be the difference from one clock frequency to another if both can achieve a correct divider for baudrate = 115200 ?
The difference is in the the Freq drift over the whole temperature range.
The most accurate clock source has the less probability to produce Frame Errors