Question
STM32F746-Disco - QSPI Failed to initialize external memory inside Cube IDE but all there are no problems using ST-LINK
This is my configuration in the include file (settings2.h) with the data to fix in the QSPI during the program phase
#ifndef IMG_NO_DATA
#if defined ( __ICCARM__ )
#pragma location = ".textqspi"
#else
__attribute__((section(".textqspi")))
#endif
const unsigned char text1[100000] = "pippo";
#else
extern const unsigned char text1[];
#endifmain_image.c
#include "settings2.h"
void dummy_init (void);
void dummy_init (void)
{
}in the main.c
#include "stm32746g_discovery_qspi.h"
#define IMG_NO_DATA
#include "settings2.h"
main()
....
char buf[1000], buf1[1000];
QSPI_HandleTypeDef hqspi;
hqspi.Instance = QUADSPI;
hqspi.Init.ClockPrescaler = 255;
hqspi.Init.FifoThreshold = 1;
hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE;
hqspi.Init.FlashSize = 1;
hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_1_CYCLE;
hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;
hqspi.Init.FlashID = QSPI_FLASH_ID_1;
hqspi.Init.DualFlash = QSPI_DUALFLASH_DISABLE;
if (HAL_QSPI_Init(&hqspi) != HAL_OK)
{
Error_Handler();
}
int status = BSP_QSPI_Init();
if (status == QSPI_NOT_SUPPORTED)
{
BSP_LCD_DisplayStringAt(20, 10, (uint8_t*)"QSPI Initialization : FAILED.", LEFT_MODE);
}
else if (status == QSPI_ERROR)
{
BSP_LCD_DisplayStringAt(20, 10, (uint8_t*)"QSPI Initialization : FAILED.", LEFT_MODE);
}
else
{
BSP_LCD_DisplayStringAt(20, 10, (uint8_t*)"QSPI Initialization : OK.", LEFT_MODE);
}
QSPI_Info QspiInfo;
/* Clear the structure */
QspiInfo.FlashSize = (uint32_t)0x00;
QspiInfo.EraseSectorSize = (uint32_t)0x00;
QspiInfo.EraseSectorsNumber = (uint32_t)0x00;
QspiInfo.ProgPageSize = (uint32_t)0x00;
QspiInfo.ProgPagesNumber = (uint32_t)0x00;
BSP_QSPI_GetInfo(&QspiInfo);
sprintf(buf, "FlashSize = %d", QspiInfo.FlashSize);
BSP_LCD_DisplayStringAt(20, 30, (uint8_t*)buf, LEFT_MODE);
sprintf(buf, "ProgPageSize = %d", QspiInfo.ProgPageSize);
BSP_LCD_DisplayStringAt(20, 50, (uint8_t*)buf, LEFT_MODE);
sprintf(buf, "ProgPagesNumber = %d", QspiInfo.ProgPagesNumber);
BSP_QSPI_MemoryMappedMode();
sprintf(buf, "Text2 = (%s) ", text1);
BSP_LCD_DisplayStringAt(20, 120, (uint8_t*)buf, LEFT_MODE);in the STM32F746NGHx_FLASH.ld
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1024K
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 307K
QSPI (xrw) : ORIGIN = 0x90000000, LENGTH = 16M <<<<<<<<<< add this entry
Memory_B1(xrw) : ORIGIN = 0x2004C000, LENGTH = 0x80
Memory_B2(xrw) : ORIGIN = 0x2004C080, LENGTH = 0x80
Memory_B3(xrw) : ORIGIN = 0x2004C100, LENGTH = 0x17d0
Memory_B4(xrw) : ORIGIN = 0x2004D8D0, LENGTH = 0x17d0
}
/* Define output sections */
SECTIONS
{
/* The startup code goes first into FLASH */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH
.textqspi : <<<<<<<<<< add this section
{
. = ALIGN(4);
_qspi_start = .; /* create a global symbol at qspi start */
*(.textqspi) /* .textqspi sections */
*(.textqspi*) /* .textqspi* sections */
. = ALIGN(4);
_qspi_end = .; /* define a global symbols at end of textqspi */
} >QSPI AT> FLASH
/* The program code and other data goes into FLASH */
.text :
{
...
.ARM.attributes 0 : { *(.ARM.attributes) }
.textqspi : { *(.textqspi) } >QSPI <<<<<<<<<<<<<<<<<<<<<<<<<< add this entry
.RxDecripSection : { *(.RxDescripSection) } >Memory_B1
.TxDescripSection : { *(.TxDescripSection) } >Memory_B2
.RxarraySection : { *(.RxBUF) } >Memory_B3
.TxarraySection : { *(.TxBUF) } >Memory_B4
}and this setting N25Q128_STM32F746-DISCO
the compile phase now it is ok
I see the QSPI data in the STM32746G_Ver31.map
but I get the error during the flash phase of the external QSPI
STMicroelectronics ST-LINK GDB server. Version 5.7.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Failed to initialize external memory!
Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target.solved with ST-LINK Server and this settings